Other Parts Discussed in Thread: TMS320C6678
Hello:
I'm developing two types of board, one with two C6678 and another with five C6678. The JTAG interface is 14 pins connector, and the level is 3.3v.
Which types of emulator can be used when debugging? XDS100, XDS560 or XDS 560V2. Which is the best one?
And, if CCS5 is must selected for C6678?
Regard,
Guoman