Can u suggest an HDMI Monitor which can be used with netra EVM.
I wan to develop touch screen applications on NETRA.
Can I use this HDMI Monitor with NETRA EVM(DM816x/C6A816x/AM389x EVM)
http://www.lilliputuk.com/monitors/hdmi/fa1011/
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can u suggest an HDMI Monitor which can be used with netra EVM.
I wan to develop touch screen applications on NETRA.
Can I use this HDMI Monitor with NETRA EVM(DM816x/C6A816x/AM389x EVM)
http://www.lilliputuk.com/monitors/hdmi/fa1011/
Hi,
This monitor can be used as it can take HDMI as well as DVI. All HDMI compatible monitors should work with Netra EVM as such.
Regards,
Hardik Shah
If the monitor touch screen generates a USB mouse compatible output then you can connect this to Netra for the touch screen interface.
Any monitor which accepts DVI/HDMI and uses USB mouse emulation for its touch screen should be good.
BR,
Steve
Hi,
This monitor is VGA monitor like old PC monitors which can take VGA signals in. There is no HDMI or DVI input to this monitor. DM8168 will support on VGA output. But if you want to drive two displays, you will have to use monitor with HDMI/DVI in or put an exteranal DAC chip after DVO2 output to convert DVO signals to analog VGA signals. Earlier monitor which you were asking is much better than this.
Regards,
Hardik Shah
Hi,
This should work with DM816x. It is better since it has HDMI/DVI and VGA support. Further it supports upto 1080P resolution also. Specifications says it supports 1080P. Please confirm with manufacturer that it will support 1080P60 along with 1080p30. As such DM816x supports 1080P30 and 1080p60 both.
Regards,
Hardik Shah