This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what's the ability of omap3530 ISP ITU.656 mode?

Other Parts Discussed in Thread: OMAP3530

Hello, Dear TI expert,

 

     we'are thinking use oma3530 ISP interface as 656 mode to support multiple video flow(CIF or D1), ideally we hope to support 4 CIF flow simutaneously.

But the datasheet has stated the 656 mode can only support 75MHz at most. And the datasheet also said "The camera subsystem supports up to two simultaneous pixel flows but only one of them can use the video processing hardware", then what's kind of the pixel flow it refers? D1? HD?

Technically, it seems OMAP3530 656 mode can support 3 CIF flow simutaneously, am I right? 

 

Any comments from your side is appreciated !

 

BR