Part Number: AM4372
Dear experts,
I want to use 2x AM437x in my design.
To create some kind of Synchronization between those I would like to use the mcSPI-Interface.
My idea envisages using the 4xSPI Interface in half-duplex mode.
2-SPI interfaces shall be used as receive only slave and two senders on both sides as Master in transmit Only mode.
Both sides should buffer up to 64 byte with the help of the FIFO. Both on receiver and transmitter side.
My assumption is that a separate FIFO is available for each SPI interface. Is that correct?
Is this configuration feasible or there are hardware restrictions in this regard that you see ?
Regards,
Alex