am335x SDK version 08.02.00.24
CPSW working mode is dual mac.
eth0 cannot receive packet with VLAN ID 0.
How to configure to solve this problem ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
am335x SDK version 08.02.00.24
CPSW working mode is dual mac.
eth0 cannot receive packet with VLAN ID 0.
How to configure to solve this problem ?
Hi,
I will need to research this question. In dual mac mode VLAN IDs 0 and 1 are used to configure the CPSW for dual mac mode. I believe it is possible to pick other VLAN IDs.
Best Regards,
Schuyler
Hi,
So you are familiar with where the VLANs are being setup. Are you using a TI EVM? If not are you using the TI file system? If using the TI file system there is an app called switch-config. This app will display the contents of the ALE in the CPSW which are rules the enable traffic. The command is:
switch-config -d
Could you please list the commands that you are using to enable the VLAN ID 0?
Best Regards,
Schuyler