Part Number: AM62P
Hello,
I'm trying to perform an early boot of the MCU-R5F (boot MCU-R5F before linux) without success.
Basically, I'm trying to replicate the booting method showed in the below image, where the WKUP-R5F releases the MCU reset before booting Linux.

I modified my R5 device tree with the alias of my new remoteproc and added the R5F driver in the SPL defconfig, but I can't get it to initialize.

I have this log:
U-Boot SPL 2023.04 (Feb 28 2024 - 18:30:33 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
SPL initial stack usage: 17040 bytes
Trying to boot from MMC1
Authentication passed
Authentication passed
Authentication passed
rproc_pre_probe: 'a53@0': using fdt
k3_arm64 a53@0: k3_arm64_probe
k3_arm64 a53@0: k3_arm64_of_to_priv
k3_arm64 a53@0: ti_sci_proc_of_to_priv
k3_arm64 a53@0: Remoteproc successfully probed
k3_arm64 a53@0: k3_arm64_init
k3_arm64 a53@0: k3_arm64_init: rproc successfully initialized
rproc_load: Loading to 'a53@0' from address 0x00000000 size of 2658664448 bytes
k3_arm64 a53@0: k3_arm64_load addr = 0x9e780000, size = 0x200
ti_sci_proc_request: proc_id = 32
k3_arm64 a53@0: GTC RATE= 200000000
ti_sci_proc_set_config: proc_id = 32, boot_vector = 0xx, cfg_set = 0x43c12c61, cfg_clr = 0x9e780000
Authentication passed
Authentication passed
Starting ATF on ARM64 core...
Are the steps executed correct? I couldn't find documentation regarding this.
Thanks,
Franco