This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 Log_printf SeqID not continuous



Hi

CCSv4.2.4.

The seqID is not continuous in the logger buffer (see numbers in RED). I only have one instance of the logger buffer, so how can it not be continuous?

"9,096,712,224",44,**** Boss: MCMGR_IPC_MSG_START_DONE_CMD #101,
"9,096,712,430",45,MultiCoreMgr_completedStart: CoreIDx 0 CMD 16 Cycle counts: 128 ,
"9,192,240,732",46,MultiCoreMgr Start Sequence Completed,
"9,192,251,322",47,---HOSTMGR Start time 11588230
"28,612,950,457",84160,"DopAtFft: nsamps=216, numCbufPacks=9",
"28,613,058,732",84161,"Dop nq 1: t= 156, nsamps=24 tsamps=1564248"
"28,613,076,727",84162,"ResampFilt: in 216 samps, out 144 samps",
"28,613,106,938",84163,"Audio: in 14 samps, out 54 samps"

Cheers

Eddie