This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDX654IDKEVM: the PRU ICSSG interfaces bounce between link states with PHYs in interrupt mode

Part Number: TMDX654IDKEVM

Hello,

the PRU ICSSG interfaces bounce between link states with PHYs in interrupt mode

The issue is reproducible by controlling interface state. In a few repeating calls "if l set eth3 down", "if l set eth3 up" occurs link state bouncing for some time.

HW setup
TMDX654IDKEVM PROC062B and loopback connection between 2 bottom ICSSG ports.

SW setup
Image from SDK 09.01.00.01 (~/ti-processor-sdk-linux-rt-am65xx-evm-09.01.00.01/filesystem/am65xx-evm/tisdk-default-image-am65xx-evm.wic.xz)
 - With altered DeviceTree with fix and configured PHY interrupt mode for all PRU ICSSGs - prepared according to upstream patch (https://lore.kernel.org/all/20231215054721.1975642-1-s-vadapalli@ti.com/)
 - Used DeviceTree patch for kernel in SDK 09.01.00.01 is in file "dt.patch"
 - See "LOG patched DT image link bouncing.txt" the link is bouncing between up and down for some time

U-Boot SPL 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
SPL initial stack usage: 1424 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty
NOTICE:  BL31: Built : 09:34:15, Aug 24 2023
I/TC:
I/TC: OP-TEE version: 4.0.0 (gcc version 11.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted


U-Boot 2023.04-gc1c2bdf272 (Nov 30 2023 - 18:17:44 +0000)

SoC:   AM65X SR2.0 GP
Model: Texas Instruments AM654 Base Board
Board: AM6-COMPROCEVM rev B
DRAM:  4 GiB
Core:  119 devices, 31 uclasses, devicetree: separate
MMC:   mmc@4f80000: 0, mmc@4fa0000: 1
Loading Environment from nowhere... OK
In:    serial
Out:   serial
Err:   serial
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00102 cpsw_ver: 0x6BA80102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: AM6-IDKAPPEVM rev A
Detected: SER-PCIE2LEVM rev A
Net:   eth0: ethernet@46000000port@1
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
574 bytes read in 26 ms (21.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
## Error: "main_cpsw0_qsgmii_phyinit" not defined
19241472 bytes read in 222 ms (82.7 MiB/s)
66677 bytes read in 28 ms (2.3 MiB/s)
Working FDT set to 88000000
10423 bytes read in 28 ms (363.3 KiB/s)
2333 bytes read in 28 ms (81.1 KiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008feec000, end 000000008fffffff ... OK
Working FDT set to 8feec000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.1.46-rt13-gb4f1767f9e (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT_RT Thu Nov 30 22:21:00 UTC 2023
[    0.000000] Machine model: Texas Instruments AM654 Base Board
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a20fffff]
[    0.000000]   node   0: [mem 0x00000000a2100000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[    0.000000] cma: Reserved 32 MiB at 0x00000000fe000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.4
[    0.000000] percpu: Embedded 19 pages/cpu s37696 r8192 d31936 u77824
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032192
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=06f70d59-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x00000000fa000000-0x00000000fe000000] (64MB)
[    0.000000] Memory: 3945104K/4194304K available (11584K kernel code, 1254K rwdata, 3944K rodata, 1856K init, 461K bss, 216432K reserved, 32768K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[    0.000000] rcu:     RCU priority boosting: priority 1 delay 500 ms.
[    0.000000] rcu:     RCU_SOFTIRQ processing moved to rcuc kthreads.
[    0.000000]  No expedited grace period (rcu_normal_after_boot).
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 100 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000880040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
[    0.000000] rcu:     Offload RCU callbacks from CPUs: 0-3.
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.000496] Console: colour dummy device 80x25
[    0.457598] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=200000)
[    0.457612] pid_max: default: 32768 minimum: 301
[    0.457707] LSM: Security Framework initializing
[    0.457874] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.457904] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.460366] cblist_init_generic: Setting adjustable number of callback queues.
[    0.503563] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.509917] cblist_init_generic: Setting adjustable number of callback queues.
[    0.517334] cblist_init_generic: Setting shift to 2 and lim to 1.
[    0.524068] rcu: Hierarchical SRCU implementation.
[    0.524072] rcu:     Max phase no-delay instances is 400.
[    0.524155] printk: bootconsole [ns16550a0] printing thread started
[    0.541614] Platform MSI: msi-controller@1820000 domain created
[    0.541921] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.542344] EFI services will not be available.
[    0.542778] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.577101] Detected VIPT I-cache on CPU1
[    0.577241] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[    0.577261] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
[    0.577321] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
I/TC: Secondary CPU 2 initializing
I/TC: Secondary CPU 2 switching to normal world boot
[    0.612642] Detected VIPT I-cache on CPU2
[    0.612868] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000
[    0.612888] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000
[    0.612947] CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
I/TC: Secondary CPU 3 initializing
I/TC: Secondary CPU 3 switching to normal world boot
[    0.648199] Detected VIPT I-cache on CPU3
[    0.648303] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000
[    0.648319] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000
[    0.648355] CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
[    0.648524] smp: Brought up 1 node, 4 CPUs
[    0.678189] SMP: Total of 4 processors activated.
[    0.678197] CPU features: detected: 32-bit EL0 Support
[    0.678203] CPU features: detected: CRC32 instructions
[    0.678282] CPU: All CPU(s) started at EL2
[    0.678285] alternatives: applying system-wide alternatives
[    0.680675] devtmpfs: initialized
[    0.700346] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 1911260446275000 ns
[    0.700374] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.701802] pinctrl core: initialized pinctrl subsystem
[    0.702562] DMI not present or invalid.
[    0.703416] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.717457] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.718011] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.718358] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.718493] audit: initializing netlink subsys (disabled)
[    0.718742] audit: type=2000 audit(0.713:1): state=initialized audit_enabled=0 res=1
[    0.719446] thermal_sys: Registered thermal governor 'step_wise'
[    0.719704] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.757086] ASID allocator initialised with 65536 entries
[    0.772715] platform 900000.serdes: Fixed dependency cycle(s) with /bus@100000/serdes@910000
[    0.785017] KASLR disabled due to lack of seed
[    0.798938] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.798949] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.798956] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.798961] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.798967] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.798971] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.798976] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.798980] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.806762] k3-chipinfo 43000014.chipid: Family:AM65X rev:SR2.0 JTAGID[0x1bb5a02f] Detected
[    0.808374] iommu: Default domain type: Translated
[    0.808381] iommu: DMA domain TLB invalidation policy: strict mode
[    0.808869] SCSI subsystem initialized
[    0.809344] usbcore: registered new interface driver usbfs
[    0.809401] usbcore: registered new interface driver hub
[    0.809443] usbcore: registered new device driver usb
[    0.810069] pps_core: LinuxPPS API ver. 1 registered
[    0.810073] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.810094] PTP clock support registered
[    0.810316] EDAC MC: Ver: 3.0.0
[    0.811563] FPGA manager framework
[    0.811695] Advanced Linux Sound Architecture Driver Initialized.
[    0.813032] clocksource: Switched to clocksource arch_sys_counter
[    0.813349] VFS: Disk quotas dquot_6.6.0
[    0.813404] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.824935] NET: Registered PF_INET protocol family
[    0.825394] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
 b   0.829832] tcp_listen_portaddr_hash hashI /TtCa:b leRe senertvriede ssh:a r20e4d8 m (emoorrdey ri: s4 e, na8b1l9e20d
  ytIes/,TC l: iDnyeanra)mi
tu[ sh a re d0. m8e29mo99r4y] i Tsa benlae-blpeedr
lirbI /haTCsh:  tNoabrlmae le Wnotrrilde s:v i6rt5u5al3i6 z(atoridoen r:su 6p,p o2rt62 i14s4  dbisyateblse,d
: neIa/TrC)
l A[ sy  nc h0r.o83n0o0u4s 1n] otTCiPfi ceasttiabonlsi shaered  hdiassahbl etadb
 e entries: 32768 (order: 6, 262144 bytes, linear)
[    0.830658] TCP bind hash table entries: 32768 (order: 9, 2621440 bytes, linear)
[    0.833842] TCP: Hash tables configured (established 32768 bind 32768)
[    0.834133] UDP hash table entries: 2048 (order: 5, 196608 bytes, linear)
[    0.834389] UDP-Lite hash table entries: 2048 (order: 5, 196608 bytes, linear)
[    0.834873] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.835701] RPC: Registered named UNIX socket transport module.
[    0.835708] RPC: Registered udp transport module.
[    0.835712] RPC: Registered tcp transport module.
[    0.835716] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.835726] NET: Registered PF_XDP protocol family
[    0.835749] PCI: CLS 0 bytes, default 64
[    0.844074] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[    0.846466] Initialise system trusted keyrings
[    0.846767] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[    0.856949] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.857741] NFS: Registering the id_resolver key type
[    0.857804] Key type id_resolver registered
[    0.857809] Key type id_legacy registered
[    0.857918] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.857925] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.914916] Key type asymmetric registered
[    0.914931] Asymmetric key parser 'x509' registered
[    0.915060] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[    0.915259] io scheduler mq-deadline registered
[    0.915266] io scheduler kyber registered
[    0.924297] pinctrl-single 4301c000.pinctrl: 70 pins, size 280
[    0.925170] pinctrl-single 11c000.pinctrl: 185 pins, size 740
[    0.925468] pinctrl-single 11c2e8.pinctrl: 9 pins, size 36
[    0.936500] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[    0.953529] loop: module loaded
[    0.955330] megasas: 07.719.03.00-rc1
[    0.960893] tun: Universal TUN/TAP device driver, 1.6
[    0.962117] thunder_xcv, ver 1.0
[    0.962175] thunder_bgx, ver 1.0
[    0.962228] nicpf, ver 1.0
[    0.962517] e1000: Intel(R) PRO/1000 Network Driver
[    0.962521] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    0.962585] e1000e: Intel(R) PRO/1000 Network Driver
[    0.962588] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    0.962646] igb: Intel(R) Gigabit Ethernet Network Driver
[    0.962650] igb: Copyright (c) 2007-2014 Intel Corporation.
[    0.962700] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.962705] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.962903] sky2: driver version 1.30
[    0.964166] VFIO - User Level meta-driver version: 0.3
[    0.965296] usbcore: registered new interface driver usb-storage
[    0.966253] i2c_dev: i2c /dev entries driver
[    0.967128] sdhci: Secure Digital Host Controller Interface driver
[    0.967132] sdhci: Copyright(c) Pierre Ossman
[    0.967480] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.968645] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.969179] usbcore: registered new interface driver usbhid
[    0.969184] usbhid: USB HID core driver
[    0.970616] optee: probing for conduit method.
[    0.970644] optee: revision 4.0 (2a5b1d12)
[    1.003516] optee: dynamic shared memory is enabled
[    1.004111] optee: initialized driver
[    1.007001] Initializing XFRM netlink socket
[    1.007107] NET: Registered PF_PACKET protocol family
[    1.007223] Key type dns_resolver registered
[    1.007555] registered taskstats version 1
[    1.007593] Loading compiled-in X.509 certificates
[    1.024646] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
[    1.098839] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[    1.100085] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz
[    1.101418] pca953x 2-0021: supply vcc not found, using dummy regulator
[    1.101584] pca953x 2-0021: using no AI
[    1.113892] omap_i2c 2000000.i2c: bus 2 rev0.12 at 400 kHz
[    1.114963] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHz
[    1.116044] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz
[    1.116421] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 156 domain created
[    1.116704] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 100 domain created
[    1.116965] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 182 domain created
[    1.117479] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 179 created
[    1.127748] OF: /bus@100000/pcie@5500000: phandle pcie-mode@4060 needs 1, found 0
[    1.128211] keystone-pcie 5500000.pcie: host bridge /bus@100000/pcie@5500000 ranges:
[    1.128276] keystone-pcie 5500000.pcie:       IO 0x0010020000..0x001002ffff -> 0x0000000000
[    1.128306] keystone-pcie 5500000.pcie:      MEM 0x0010030000..0x0017ffffff -> 0x0010030000
[    1.128621] OF: /bus@100000/pcie@5500000: phandle pcie-devid@210 needs 1, found 0
[    1.128676] keystone-pcie 5500000.pcie: iATU unroll: enabled
[    1.128683] keystone-pcie 5500000.pcie: iATU regions: 8 ob, 8 ib, align 64K, limit 4G
[    2.128996] keystone-pcie 5500000.pcie: Phy link never came up
[    2.129263] keystone-pcie 5500000.pcie: PCI host bridge to bus 0000:00
[    2.129276] pci_bus 0000:00: root bus resource [bus 00-ff]
[    [2.147661] printk: console [ttyS2] printing thread started
    2.129287] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    2.147685] printk: console [ttyS2] enabled
[    2.147694] printk: bootconsole [ns16550a0] disabled
[    2.159630] printk: bootconsole [ns16550a0] printing thread stopped
[    2.166538] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    2.201083] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.202785] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    2.202844] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[    2.203006] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    2.203058] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    2.204402] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    2.208622] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    2.210840] mmc0: CQHCI version 5.10
[    2.225963] pca953x 0-0039: supply vcc not found, using dummy regulator
[    2.226216] pca953x 0-0039: using no AI
[    2.239903] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[    2.240486] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[    2.242835] ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16)
[    2.251533] ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64)
[    2.253348] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    2.267899] spi-nor spi0.0: mt35xu512aba (65536 Kbytes)
[    2.268059] 8 fixed-partitions partitions found on MTD device 47040000.spi.0
[    2.268072] Creating 8 MTD partitions on "47040000.spi.0":
[    2.268081] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    2.270131] 0x000000080000-0x000000280000 : "ospi.tispl"
[    2.271928] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    2.273821] 0x000000680000-0x0000006a0000 : "ospi.env"
[    2.275606] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[    2.277359] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[    2.279082] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    2.280812] 0x000003fe0000-0x000004000000 : "ospi.phypattern"
[    2.288929] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[    2.323086] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.324961] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[    2.325063] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[    2.325236] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    2.325245] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    2.326331] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    2.347000] mmc0: Command Queue Engine enabled
[    2.347061] mmc0: new HS200 MMC card at address 0001
[    2.347980] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[    2.351518] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB
[    2.352284] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    2.353611] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB
[    2.355724] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (240:0)
[    2.359386] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present!
[    2.359478] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present!
[    2.359587] mmc1: CQHCI version 5.10
[    2.363250] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    2.384837] ALSA device list:
[    2.384848]   No soundcards found.
[    2.401653] mmc1: SDHCI controller on 4fa0000.mmc [4fa0000.mmc] using ADMA 64-bit
[    2.462662] Waiting for root device PARTUUID=06f70d59-02...
[    2.714924] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[    2.715992] mmcblk1: mmc1:aaaa SM16G 14.8 GiB
[    2.719047]  mmcblk1: p1 p2
[    2.747563] EXT4-fs (mmcblk1p2): recovery complete
[    2.748200] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
[    2.748290] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    2.749047] devtmpfs: mounted
[    2.750418] Freeing unused kernel memory: 1856K
[    2.750565] Run /sbin/init as init process
[    2.903117] systemd[1]: System time before build time, advancing clock.
[    2.938947] NET: Registered PF_INET6 protocol family
[    2.940838] Segment Routing with IPv6
[    2.940892] In-situ OAM (IOAM) with IPv6
[    2.969433] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    2.970318] systemd[1]: Detected architecture arm64.

Welcome to Arago 2023.10!

[    3.055642] systemd[1]: Hostname set to <am65xx-evm>.
[    3.168967] systemd-sysv-generator[202]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    3.171108] systemd-sysv-generator[202]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    3.171450] systemd-sysv-generator[202]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    3.487088] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    3.555630] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    3.636858] systemd[1]: Queued start job for default target Graphical Interface.
[  OK  ] Created slice Slice /system/getty    3.795256] systemd[1]: Created slice Slice /system/getty.
0m.
[  OK  ] Created slice Slice /system/modprob[    3.813664] systemd[1]: Created slice Slice /system/modprobe.
e.
[  OK  ] Created slice Slice /system/serial-[    3.832465] systemd[1]: Created slice Slice /system/serial-getty.
getty.
[    3.850830] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Started Dispatch Password …ts to [    3.865673] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
Console Directory Watch.
[  OK  ] Started Forward Password R…uests [    3.882681] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
to Wall Directory Watch.
[  OK  ] Reached target Path Units.
[    3.899652] systemd[1]: Reached target Path Units.
[  OK  ] Reached target Remote File Systems systemd[1]: Reached target Remote File Systems.
[0m.
[  OK  ] Reached target Slice Units.
[    3.924252] systemd[1]: Reached target Slice Units.
[    3.934908] systemd[1]: Reached target Swaps.
[  OK  ] Reached target Swaps.
[  OK  ] Listening on RPCbind Server Activat[    4.000327] systemd[1]: Listening on RPCbind Server Activation Socket.
ion Socket.
[  OK  ] Reached target RPC Port Mapper.[    4.015440] systemd[1]: Reached target RPC Port Mapper.

[  OK  ] Listening on Process Core Dump Sock[    4.040658] systemd[1]: Listening on Process Core Dump Socket.
et.
[  OK  ] Listening on initctl Compatibility [    4.055726] systemd[1]: Listening on initctl Compatibility Named Pipe.
Named Pipe.
[  OK  ] Listening on Journal Audit Socket    4.072353] systemd[1]: Listening on Journal Audit Socket.
0m.
[    4.086996] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    4.101974] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[  OK  ] Listening on Network Service Netlin[    4.114257] systemd[1]: Listening on Network Service Netlink Socket.
k Socket.
[  OK  ] Listening on udev Control Socket    4.130233] systemd[1]: Listening on udev Control Socket.
m.
[  OK  ] Listening on udev Kernel Socket[    4.144794] systemd[1]: Listening on udev Kernel Socket.
.
[  OK  ] Listening on User Database Manager [    4.158803] systemd[1]: Listening on User Database Manager Socket.
Socket.
[    4.194783] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
         Mounting POSIX Message Queue File System..[    4.214448] systemd[1]: Mounting POSIX Message Queue File System...
.
         Mounting Kernel Debug File System...
[    4.236656] systemd[1]: Mounting Kernel Debug File System...
[    4.248767] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
         Mounting Temporary Directory /tmp...[    4.258853] systemd[1]: Mounting Temporary Directory /tmp...

         Starting Create List of Static Device Nodes    4.285330] systemd[1]: Starting Create List of Static Device Nodes...
m...
[    4.307976] systemd[1]: Starting Load Kernel Module configfs...
         Starting Load Kernel Module configfs...
         Starting Load Kernel Module drm...
[    4.351242] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module fuse...
[    4.369522] systemd[1]: Starting Load Kernel Module fuse...
[    4.393120] fuse: init (API version 7.37)
         Starting Start psplash boot splash screen.[    4.410438] systemd[1]: Starting Start psplash boot splash screen...
..
         Starting RPC Bind...
[    4.434682] systemd[1]: Starting RPC Bind...
[    4.443790] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
         Starting Journal Service...
[    4.455577] systemd[1]: Starting Journal Service...
[    4.476731] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
         Starting Generate network …ts from Kernel co[    4.497222] systemd[1]: Starting Generate network units from Kernel command line...
mmand line...
[    4.507186] cryptodev: loading out-of-tree module taints kernel.
[    4.509319] cryptodev: driver 1.12 loaded.
         Starting Remount Root and Kernel File Systems systemd[1]: Starting Remount Root and Kernel File Systems...
[0m...
         Starting Coldplug All udev Devices...[    4.557416] systemd[1]: Starting Coldplug All udev Devices...

[    4.585248] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
[  OK  ] Started RPC Bind.[    4.591172] systemd[1]: Started RPC Bind.

[  OK  ] Mounted Huge Pages File System.[    4.605565] systemd[1]: Mounted Huge Pages File System.

[    4.619989] systemd[1]: Mounted POSIX Message Queue File System.
[  OK  ] Mounted POSIX Message Queue File System.
[    4.636989] systemd[1]: Mounted Kernel Debug File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory /tmp    4.651973] systemd[1]: Mounted Temporary Directory /tmp.
m.
[    4.668981] systemd[1]: Finished Create List of Static Device Nodes.
[  OK  ] Finished Create List of Static Device Nodes.
[    4.685978] systemd[1]: modprobe@configfs.service: Deactivated successfully.
[  OK  ] Finished Load Kernel Module configf[    4.687798] systemd[1]: Finished Load Kernel Module configfs.
s.
[  OK  ] Started Journal Service.[    4.708975] systemd[1]: Started Journal Service.

[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[  OK  ] Finished Load Kernel Modules.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting FUSE Control File System...
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
[    4.919826] systemd-journald[218]: Received client request to flush runtime journal.
         Starting Apply Kernel Variables...
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted FUSE Control File System.
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /media/ram...
         Mounting /var/volatile...
[    5.110441] audit: type=1334 audit(1651167747.208:2): prog-id=5 op=LOAD
[    5.110679] audit: type=1334 audit(1651167747.208:3): prog-id=6 op=LOAD
         Starting Rule-based Manage…for Device Events and Files...
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Create Volatile Files and Directories.
[  OK  ] Started Rule-based Manager for Device Events and Files.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[  OK  ] Finished Coldplug All udev Devices.
[    5.534119] random: crng init done
[  OK  ] Finished Load/Save Random Seed.
[  OK  ] Found device /dev/ttyS2.
[    5.942748] spi-nor spi2.0: n25q128a13 (16384 Kbytes)
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Started Daily rotation of log files.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[    6.048114] CAN device driver interface
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
[  OK  ] Listening on dropbear.socket.
[  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
         Starting Weston socket...
         Starting Console System Startup Logging...
         Starting D-Bus System Message Bus...
         Starting Reboot and dump vmcore via kexec...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Listening on Weston socket.
[  OK  ] Finished Console System Startup Logging.
[  OK  ] Finished Reboot and dump vmcore via[    6.282716] [drm] Initialized pvr 1.17.4948957 20110701 for 7000000.gpu on minor 0
 kexec.
[  OK  ] Reached target Socket Units.
[    6.420044] platform 41000000.r5f: configured R5F for remoteproc mode
[    6.421132] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[    6.421569] remoteproc remoteproc0: 41000000.r5f is available
[    6.427271] remoteproc remoteproc0: powering up 41000000.r5f
[    6.427298] remoteproc remoteproc0: Booting fw image am65x-mcu-r5f0_0-fw, size 82412
[    6.446594] rproc-virtio rproc-virtio.2.auto: assigned reserved memory node r5f-dma-memory@a0000000
[    6.447567] virtio_rpmsg_bus virtio0: rpmsg host is online
[    6.447615] rproc-virtio rproc-virtio.2.auto: registered virtio0 (type 7)
[    6.447626] remoteproc remoteproc0: remote processor 41000000.r5f is now up
[    6.467345] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    6.467661] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    6.494263] davinci_mdio b032400.mdio: Configuring MDIO in manual mode
[    6.537593] davinci_mdio b032400.mdio: davinci mdio revision 1.7, bus freq 1000000
[    6.589908] davinci_mdio b032400.mdio: phy[0]: device b032400.mdio:00, driver TI DP83867
[    6.589929] davinci_mdio b032400.mdio: phy[3]: device b032400.mdio:03, driver TI DP83867
[    6.699781] davinci_mdio b132400.mdio: Configuring MDIO in manual mode
[  OK  ] Started D-Bus System Message Bus.
[    6.737121] davinci_mdio b132400.mdio: davinci mdio revision 1.7, bus freq 1000000
[  OK  ] Reached target Basic System.
[  OK  ] Started Job spooling tools.
[  OK  ] Started Periodic Command Scheduler.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
[  OK  ] Started irqbalance daemon.
[    6.931960] m_can_platform 40528000.mcan: m_can device registered (irq=585, version=32)
[    6.935799] m_can_platform 40568000.mcan: m_can device registered (irq=586, version=32)
[    6.951306] davinci_mdio b132400.mdio: phy[0]: device b132400.mdio:00, driver TI DP83867
[    6.951330] davinci_mdio b132400.mdio: phy[3]: device b132400.mdio:03, driver TI DP83867
         Starting Telephony service...
[  OK  ] Started strongSwan IPsec I…IKEv2 daemon using ipsec.conf.
[    7.044968] audit: type=1334 audit(1651191838.371:4): prog-id=7 op=LOAD
[    7.045607] audit: type=1334 audit(1651191838.372:5): prog-id=8 op=LOAD
[    7.064464] davinci_mdio b232400.mdio: Configuring MDIO in manual mode
         Starting User Login Management...
[    7.099102] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000
[  OK  ] Started TEE Supplicant.
         Starting Telnet Server...
[    7.229614] Bluetooth: Core ver 2.22
[    7.229762] NET: Registered PF_BLUETOOTH protocol family
[    7.229767] Bluetooth: HCI device and connection manager initialized
[    7.229795] Bluetooth: HCI socket layer initialized
[FAILED] Failed to start Print notice abou[    7.229808] Bluetooth: L2CAP socket layer initialized
t GPLv3 packages.
[    7.229836] Bluetooth: SCO socket layer initialized
See 'systemctl status gplv3-notice.service' for details.
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[    7.387736] davinci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver TI DP83867
[    7.387759] davinci_mdio b232400.mdio: phy[3]: device b232400.mdio:03, driver TI DP83867
[  OK  ] Finished Telnet Server.
[    7.497618] remoteproc remoteproc1: b00a000.txpru is available
[    7.498367] remoteproc remoteproc2: b00c000.txpru is available
[    7.499118] remoteproc remoteproc3: b10a000.txpru is available
[    7.504218] remoteproc remoteproc4: b10c000.txpru is available
[  OK  ] Started Telephony service.
[    7.504956] remoteproc remoteproc5: b20a000.txpru is available
[    7.506294] remoteproc remoteproc6: b20c000.txpru is available
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Started User Login Management.
[    8.002224] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    8.028622] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[  OK  ] Started Network Configuration.
[    8.213224] remoteproc remoteproc7: b006000.rtu is available
         Starting Network Name Resolution...
[    8.239815] remoteproc remoteproc8: b034000.pru is available
[    8.284180] remoteproc remoteproc9: b004000.rtu is available
[    8.286703] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[    8.286734] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[    8.296699] remoteproc remoteproc10: b038000.pru is available
[    8.300118] remoteproc remoteproc11: b134000.pru is available
[    8.302549] remoteproc remoteproc12: b104000.rtu is available
[    8.305476] remoteproc remoteproc13: b234000.pru is available
[    8.307193] remoteproc remoteproc14: b204000.rtu is available
[    8.309728] remoteproc remoteproc15: b138000.pru is available
[    8.311878] remoteproc remoteproc16: b106000.rtu is available
[    8.315082] remoteproc remoteproc17: b238000.pru is available
[    8.335011] remoteproc remoteproc18: b206000.rtu is available
[    8.461306] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[    8.728566] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    8.728635] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 1
[    8.728783] xhci-hcd xhci-hcd.3.auto: hcc params 0x0298fe6d hci version 0x110 quirks 0x0000000000010010
[    8.738196] xhci-hcd xhci-hcd.3.auto: irq 587, io mem 0x04010000
[    8.740551] xhci-hcd xhci-hcd.3.auto: xHCI Host Controller
[    8.740599] xhci-hcd xhci-hcd.3.auto: new USB bus registered, assigned bus number 2
[    8.740625] xhci-hcd xhci-hcd.3.auto: Host supports USB 3.0 SuperSpeed
[    8.776537] hub 1-0:1.0: USB hub found
[    8.776627] hub 1-0:1.0: 1 port detected
[    8.794332] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    8.836988] hub 2-0:1.0: USB hub found
[    8.837177] hub 2-0:1.0: 1 port detected
[  OK  ] Reached target Hardware activated USB gadget.
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting Enable and configure wl18xx bluetooth stack...
         Starting containerd container runtime...
[  OK  ] Started Netperf Benchmark Server.
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
         Starting Permit User Sessions...
[FAILED] Failed to start Enable and…figure wl18xx bluetooth stack.
See 'systemctl status bt-enable.service' for details.
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
         Starting Weston, a Wayland…ositor, as a system service...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[  OK  ] Created slice Slice /system/systemd-fsck.
[    9.535464] audit: type=1334 audit(1651191840.862:6): prog-id=9 op=LOAD
[    9.535747] audit: type=1334 audit(1651191840.862:7): prog-id=10 op=LOAD
         Starting User Database Manager...
[  OK  ] Found device /dev/mmcblk1p1.
         Starting File System Check on /dev/mmcblk1p1...
[  OK  ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
[  OK  ] Finished File System Check on /dev/mmcblk1p1.
         Mounting /run/media/boot-mmcblk1p1...
[  OK  ] Started User Database Manager.
[  OK  ] Mounted /run/media/boot-mmcblk1p1.
[  OK  ] Created slice User Slice of UID 1000.
         Starting User Runtime Directory /run/user/1000...
[  OK  ] Finished User Runtime Directory /run/user/1000.
         Starting User Manager for UID 1000...
[   10.148784] audit: type=1006 audit(1651191841.475:8): pid=686 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
[   10.148824] audit: type=1300 audit(1651191841.475:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe9abad58 a2=4 a3=ffff810da020 items=0 ppid=1 pid=686 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[   10.148909] audit: type=1327 audit(1651191841.475:8): proctitle="(systemd)"
[  OK  ] Started containerd container runtime.
[  OK  ] Reached target Multi-User System.
[  OK  ] Started User Manager for UID 1000.
[  OK  ] Started Session c1 of User weston.
[   11.149214] audit: type=1006 audit(1651191842.476:9): pid=650 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
[   11.149247] audit: type=1300 audit(1651191842.476:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe9abad58 a2=4 a3=ffff810da020 items=0 ppid=1 pid=650 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[   11.149269] audit: type=1327 audit(1651191842.476:9): proctitle="(weston)"
[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.
[  OK  ] Reached target Graphical Interface.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Finished Record Runlevel Change in UTMP.

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project am65xx-evm -

Arago 2023.10 am65xx-evm -

am65xx-evm login: [   18.934766] TI DP83867 b232400.mdio:00: attached PHY driver (mii_bus:phy_addr=b232400.mdio:00, irq=419)
[   18.947528] TI DP83867 b232400.mdio:03: attached PHY driver (mii_bus:phy_addr=b232400.mdio:03, irq=POLL)
[   18.947574] icssg-prueth icssg2-eth: TI PRU ethernet driver initialized: dual EMAC mode
[   18.976773] TI DP83867 b132400.mdio:00: attached PHY driver (mii_bus:phy_addr=b132400.mdio:00, irq=391)
[   18.990841] TI DP83867 b132400.mdio:03: attached PHY driver (mii_bus:phy_addr=b132400.mdio:03, irq=POLL)
[   18.990891] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: dual EMAC mode
[   19.027902] TI DP83867 b032400.mdio:00: attached PHY driver (mii_bus:phy_addr=b032400.mdio:00, irq=371)
[   19.048390] TI DP83867 b032400.mdio:03: attached PHY driver (mii_bus:phy_addr=b032400.mdio:03, irq=POLL)
[   19.105577] remoteproc remoteproc11: powering up b134000.pru
[   19.113214] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 40936
[   19.113263] remoteproc remoteproc11: unsupported resource 5
[   19.113299] remoteproc remoteproc11: remote processor b134000.pru is now up
[   19.113350] remoteproc remoteproc12: powering up b104000.rtu
[   19.115851] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30884
[   19.115911] remoteproc remoteproc12: remote processor b104000.rtu is now up
[   19.115959] remoteproc remoteproc3: powering up b10a000.txpru
[   19.118197] remoteproc remoteproc3: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36672
[   19.118259] remoteproc remoteproc3: remote processor b10a000.txpru is now up
[   19.118645] remoteproc remoteproc15: powering up b138000.pru
[   19.119992] remoteproc remoteproc15: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 41208
[   19.120062] remoteproc remoteproc15: unsupported resource 5
[   19.120097] remoteproc remoteproc15: remote processor b138000.pru is now up
[   19.120142] remoteproc remoteproc16: powering up b106000.rtu
[   19.121248] remoteproc remoteproc16: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30124
[   19.121292] remoteproc remoteproc16: remote processor b106000.rtu is now up
[   19.121328] remoteproc remoteproc4: powering up b10c000.txpru
[   19.122377] remoteproc remoteproc4: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35184
[   19.122438] remoteproc remoteproc4: remote processor b10c000.txpru is now up
[   19.123947] pps pps0: new PPS source ptp2
[   19.150365] icssg-prueth icssg0-eth: TI PRU ethernet driver initialized: dual EMAC mode
[   19.281125] remoteproc remoteproc13: powering up b234000.pru
[   19.281362] remoteproc remoteproc13: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 40936
[   19.281389] remoteproc remoteproc13: unsupported resource 5
[   19.281424] remoteproc remoteproc13: remote processor b234000.pru is now up
[   19.281462] remoteproc remoteproc14: powering up b204000.rtu
[   19.281612] remoteproc remoteproc14: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30884
[   19.281646] remoteproc remoteproc14: remote processor b204000.rtu is now up
[   19.281671] remoteproc remoteproc5: powering up b20a000.txpru
[   19.281800] remoteproc remoteproc5: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36672
[   19.281839] remoteproc remoteproc5: remote processor b20a000.txpru is now up
[   19.282332] remoteproc remoteproc17: powering up b238000.pru
[   19.282514] remoteproc remoteproc17: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 41208
[   19.282537] remoteproc remoteproc17: unsupported resource 5
[   19.282565] remoteproc remoteproc17: remote processor b238000.pru is now up
[   19.282595] remoteproc remoteproc18: powering up b206000.rtu
[   19.282743] remoteproc remoteproc18: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30124
[   19.282775] remoteproc remoteproc18: remote processor b206000.rtu is now up
[   19.282800] remoteproc remoteproc6: powering up b20c000.txpru
[   19.282922] remoteproc remoteproc6: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35184
[   19.282958] remoteproc remoteproc6: remote processor b20c000.txpru is now up
[   19.284620] pps pps1: new PPS source ptp3
[   19.486092] remoteproc remoteproc8: powering up b034000.pru
[   19.486323] remoteproc remoteproc8: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 40936
[   19.486350] remoteproc remoteproc8: unsupported resource 5
[   19.486384] remoteproc remoteproc8: remote processor b034000.pru is now up
[   19.486421] remoteproc remoteproc9: powering up b004000.rtu
[   19.486538] remoteproc remoteproc9: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30884
[   19.486571] remoteproc remoteproc9: remote processor b004000.rtu is now up
[   19.486595] remoteproc remoteproc1: powering up b00a000.txpru
[   19.486706] remoteproc remoteproc1: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36672
[   19.486743] remoteproc remoteproc1: remote processor b00a000.txpru is now up
[   19.487207] remoteproc remoteproc10: powering up b038000.pru
[   19.487343] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 41208
[   19.487365] remoteproc remoteproc10: unsupported resource 5
[   19.487396] remoteproc remoteproc10: remote processor b038000.pru is now up
[   19.487423] remoteproc remoteproc7: powering up b006000.rtu
[   19.487538] remoteproc remoteproc7: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30124
[   19.487571] remoteproc remoteproc7: remote processor b006000.rtu is now up
[   19.487595] remoteproc remoteproc2: powering up b00c000.txpru
[   19.487711] remoteproc remoteproc2: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35184
[   19.487747] remoteproc remoteproc2: remote processor b00c000.txpru is now up
[   19.489411] pps pps2: new PPS source ptp4
[   25.607791] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   25.607800] icssg-prueth icssg1-eth eth3: Link is Up - 1Gbps/Full - flow control off
[   25.607876] IPv6: ADDRCONF(NETDEV_CHANGE): eth5: link becomes ready
[   25.608330] IPv6: ADDRCONF(NETDEV_CHANGE): eth3: link becomes ready

am65xx-evm login: root
[   29.716901] audit: type=1006 audit(1651191861.043:10): pid=784 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[   29.716936] audit: type=1300 audit(1651191861.043:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe9abad58 a2=1 a3=ffff810da020 items=0 ppid=1 pid=784 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[   29.716956] audit: type=1327 audit(1651191861.043:10): proctitle="(systemd)"
[   29.749604] audit: type=1334 audit(1651191861.076:11): prog-id=11 op=LOAD
[   29.749645] audit: type=1300 audit(1651191861.076:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffca96fdc0 a2=78 a3=0 items=0 ppid=1 pid=784 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[   29.749668] audit: type=1327 audit(1651191861.076:11): proctitle="(systemd)"
[   29.749691] audit: type=1334 audit(1651191861.076:12): prog-id=11 op=UNLOAD
[   29.749829] audit: type=1334 audit(1651191861.076:13): prog-id=12 op=LOAD
[   29.749881] audit: type=1300 audit(1651191861.076:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffca96fe60 a2=78 a3=0 items=0 ppid=1 pid=784 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[   29.749904] audit: type=1327 audit(1651191861.076:13): proctitle="(systemd)"
root@am65xx-evm:~# ip l set dev eth3 down
[   38.921186] icssg-prueth icssg1-eth eth3: Link is Down
[   38.923556] icssg-prueth icssg0-eth eth5: Link is Down
root@am65xx-evm:~# ip l set dev eth3 up
root@am65xx-evm:~# [   44.137713] icssg-prueth icssg1-eth eth3: Link is Up - 1Gbps/Full - flow control off
[   44.137941] IPv6: ADDRCONF(NETDEV_CHANGE): eth3: link becomes ready
[   44.140900] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
ip l set dev eth3 down
[   45.768279] icssg-prueth icssg1-eth eth3: Link is Down
[   45.779288] icssg-prueth icssg0-eth eth5: Link is Down
[   45.787398] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.788749] icssg-prueth icssg0-eth eth5: Link is Down
[   45.790113] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.791447] icssg-prueth icssg0-eth eth5: Link is Down
[   45.795243] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.798618] icssg-prueth icssg0-eth eth5: Link is Down
[   45.800334] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.802323] icssg-prueth icssg0-eth eth5: Link is Down
[   45.809141] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.810583] icssg-prueth icssg0-eth eth5: Link is Down
[   45.812338] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.813719] icssg-prueth icssg0-eth eth5: Link is Down
[   45.815669] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.818184] icssg-prueth icssg0-eth eth5: Link is Down
[   45.819425] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.821558] icssg-prueth icssg0-eth eth5: Link is Down
[   45.822780] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.824733] icssg-prueth icssg0-eth eth5: Link is Down
[   45.827687] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.829561] icssg-prueth icssg0-eth eth5: Link is Down
[   45.833157] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.835744] icssg-prueth icssg0-eth eth5: Link is Down
[   45.838336] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.844190] icssg-prueth icssg0-eth eth5: Link is Down
[   45.846807] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.848148] icssg-prueth icssg0-eth eth5: Link is Down
[   45.854313] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.856644] icssg-prueth icssg0-eth eth5: Link is Down
[   45.858163] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.860530] icssg-prueth icssg0-eth eth5: Link is Down
[   45.863275] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.865570] icssg-prueth icssg0-eth eth5: Link is Down
[   45.866948] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.868309] icssg-prueth icssg0-eth eth5: Link is Down
[   45.869527] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.871941] icssg-prueth icssg0-eth eth5: Link is Down
[   45.873633] icssg-prueth icssg0-eth eth5: Link is Up - 1Gbps/Full - flow control off
[   45.876363] icssg-prueth icssg0-eth eth5: Link is Down
root@am65xx-evm:~#
diff --git a/arch/arm64/boot/dts/ti/k3-am654-base-board.dts b/arch/arm64/boot/dts/ti/k3-am654-base-board.dts
index b598fb278..182154566 100644
--- a/arch/arm64/boot/dts/ti/k3-am654-base-board.dts
+++ b/arch/arm64/boot/dts/ti/k3-am654-base-board.dts
@@ -666,21 +666,21 @@ &icssg1_mdio {
 
 &icssg2_mdio {
 	status = "okay";
-	pinctrl-names = "default", "icssg2-phy-irq";
-	pinctrl-0 = <&icssg2_mdio_pins_default>, <&icssg2_phy_irq_pins_default>;
+	pinctrl-names = "default";
+	pinctrl-0 = <&icssg2_mdio_pins_default>;
 
 	icssg2_phy0: ethernet-phy@0 {
+		pinctrl-names = "default";
+		pinctrl-0 = <&icssg2_phy_irq_pins_default>;
 		reg = <0>;
 		interrupt-parent = <&main_gpio1>;
-		interrupts = <87 0x2>;
+		interrupts = <87 IRQ_TYPE_EDGE_FALLING>;
 		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
 		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
 	};
 
 	icssg2_phy1: ethernet-phy@3 {
 		reg = <3>;
-		interrupt-parent = <&main_gpio1>;
-		interrupts = <87 0x2>;
 		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
 		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
 	};
diff --git a/arch/arm64/boot/dts/ti/k3-am654-idk.dtso b/arch/arm64/boot/dts/ti/k3-am654-idk.dtso
index ac45fcbfc..2a2227b66 100644
--- a/arch/arm64/boot/dts/ti/k3-am654-idk.dtso
+++ b/arch/arm64/boot/dts/ti/k3-am654-idk.dtso
@@ -9,6 +9,7 @@
 /plugin/;
 
 #include <dt-bindings/gpio/gpio.h>
+#include <dt-bindings/interrupt-controller/irq.h>
 #include <dt-bindings/net/ti-dp83867.h>
 #include "k3-pinctrl.h"
 
@@ -294,6 +295,22 @@
 	};
 };
 
+&main_pmx0 {
+	/* Select GPIO1_39 for ICSSG0 PHY interrupt */
+	icssg0_phy_irq_pins_default: icssg0-phy-irq-default-pins {
+		pinctrl-single,pins = <
+			AM65X_IOPAD(0x021c, PIN_INPUT, 7) /* (U25) PRG0_PRU_GPO10.GPIO1_39 */
+		>;
+	};
+
+	/* Select GPIO1_59 for ICSSG1 PHY interrupt */
+	icssg1_phy_irq_pins_default: icssg1-phy-irq-default-pins {
+		pinctrl-single,pins = <
+			AM65X_IOPAD(0x026c, PIN_INPUT, 7) /* (AA28) PRG0_PRU1_GPO10.GPIO1_59 */
+		>;
+	};
+};
+
 &m_can0 {
 	status = "okay";
 	pinctrl-names = "default";
@@ -316,7 +333,11 @@
 	#size-cells = <0>;
 
 	icssg0_phy0: ethernet-phy@0 {
+		pinctrl-names = "default";
+		pinctrl-0 = <&icssg0_phy_irq_pins_default>;
 		reg = <0>;
+		interrupt-parent = <&main_gpio1>;
+		interrupts = <39 IRQ_TYPE_EDGE_FALLING>;
 		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
 		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
 	};
@@ -341,7 +362,11 @@
 	#size-cells = <0>;
 
 	icssg1_phy0: ethernet-phy@0 {
+		pinctrl-names = "default";
+		pinctrl-0 = <&icssg1_phy_irq_pins_default>;
 		reg = <0>;
+		interrupt-parent = <&main_gpio1>;
+		interrupts = <59 IRQ_TYPE_EDGE_FALLING>;
 		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
 		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
 	};

Lukas Libal