There is a section on this webpage:
http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map
called "DSP for OMX".
1) Is this configuration of the memory map applicable for OpenMAX codecs running on the HDVICPs? The name makes me think it isn't, because the DSP isn't the same as the HDVICPs but I'd be grateful if someone could clear up my confusion as I don't know where OpenMAX gets its memory map configured otherwise (unless it's at the time of media controller firmware loading).
2) While I'm here, what does "patch release" mean? This is referred to several times in the above webpage.
3) Why in "<EZSDK>/component-sources/c6accel_2_01_00_09/soc/packages/ti/c6accel_unitservers/TI816X/serverplatforms.xs" does the memory map contradict all the other memory maps I've seen around? It states that Linux occupies 166MB whereas the "length" field in this file indicates that it actually occupies 268MB, and the link above says that Linux occupies 364MB whereas the default board kernel parameters suggest that Linux only has 256MB.
I am very confused.
Thanks,
Ralph