Other Parts Discussed in Thread: AM1808, AM1707
Hello,
I use AM1808 EVM with latest Sitara Linux.
Software Development Environment - CCS 5.0.3 , build tools - Code Sourcery G++ 2011.03-65.
When I try to debug my multi-threaded application on the target, I noticed the following:
1) The debugger works fine with main application thread;
2) When I set the breakpoints in other application threads, the debugger does not stop there (though I see the indication in the debugger window that the threads were activated);
3) Just to make sure that my threads are not messed up, I added printouts to STDOUT from other threads - all printouts work OK. It means there are no problems with the threads execution.
So my questions are:
1) Are there any flags, or options in the GDB to enable multi-threaded debugging?
2) What should I do to enable it?
3) If it is not possible to do with GDB, what other options do I have?
Regards,
Slavik