This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SATA and TMS320C6457

Other Parts Discussed in Thread: TMS320C6678, TMS320C6457

Whether it is possible to processors TMS320C6457 and TMS320C6678 to connect to SerialIO SATA Hard Drive Disk?

Whether there is any description as it to make?

Whether there are libraries for work with Hard Drive Disk?

  • Connected either of these devices directly to a SATA hard drive would require an internal SATA capableSERDES interface.  Neither of these two components has that interface.  You could use a different component with a SATA interface and connect to the C6457 or the C6678 using serial RapidIO but I haven't seen and example designs of that type.