This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

spi eeprom burning problem for C55

Hi all,

I have problem related to burning eeprom. I have 64KB spi eeprom on which I flashed application program. It is programmed with no error.

But when I replace it with 1Mbit(128KB)  one, I get the following error;

 

SPI EEPROM...

Writing data to device...

Opening D:\CSL_AUDIO_DRIVER.bin...

Input file opened

WRITE ERROR! at 0x0000

Wrote 0x09aa  Read 0x00ff

- I am using C5505. I know it should support 16 bit and 24 bit spi flash. Doesn't it?

- Or, what can be the reason?

I use M95M01-RMN6TP eeprom.

Thanks,