I am trying to measure the PCIe throughput of C6678 system. I have connected the C6678 EVM to a PC with the PC acting as RC and C6678 as EP.
Only IBL is running on C6678. And PC side has mapped one BAR to the DDR on C6678 and is pushing data into it. The maximum throughput i am getting is only 250MBs
which is very less compared to the fact that the link is 2x and gen2.
Can somebody help me out?