Other Parts Discussed in Thread: AM3505
Hello
I have read the wiki on setting up the EMIF4 DDR2 interface on a AM3505, see http://processors.wiki.ti.com/index.php/Setting_up_AM35x_SDRC_registers.
It mentions a VTP calibration process, which is nowhere described (TRM, wiki). It also claims, that the setup process is implemented in the am3517-evm kit software, available at:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/sdk/AM3517/latest/index_FDS.html
But then it also says that the VTP-calib step #3 is not implemented in the linux code...
Question 1: What are the steps to performa a VTP calibration?
Question 2: Is the VTP calibration process initiated by setting the VTP_DYN bit in EMIF4_DDR_PHYCTL1 ?
Question 3: Is this the complete VTP calibration process?
Thanks and kind regards,
-Urs