Dear all:
I encounter a issue that our performance reach 1080P 20FPS in DM368 platform . And we using codec 2.0 it should be 1080P 30FPS
We has reference to the way of third party ( APPRO and TI FAE suggestion ) but it still reach 1080P 20FPS. We can't understand why?
Can anyone give me any suggestion or information to resolve this issue. I grateful for that.
The following is the relevant parameters and status:
thanks for your visit
IC :
TMX320
DM365BZCE 40
YFA-99ACHPW
ours platform status as below :
ARM Hz = 432000000
DDR Hz = 340000000
VPSS Hz = 340000000
IMCOP Hz = 340000000
Create encoder algorithm with parameters as below:
1.
==========ALG_vidEncCreate VIDENC1_Params ===================
size:124
encodingPreset:3
rateControlPreset:5
maxHeight:1088
maxWidth:1920
maxFrameRate:60000
maxBitRate:12000000
dataEndianness:1
maxInterFrameInterval:1
inputChromaFormat:9
inputContentType:0
reconChromaFormat:9
===============================================
=========== ALG_PrintvidEncDynamicParams IH264VENC_DynamicParams ==========
sliceSize:0
airRate :0
intraFrameQP :28
interPFrameQP:28
initQ :28
rcQMax :51 42
rcQMin :1
rcQMaxI:51 42
rcQMinI:1
rcAlgo :1
maxDelay:2000
aspectRatioX:1
aspectRatioY:1
lfDisableIdc:0
enableBufSEI:1
enablePicTimSEI:1
perceptualRC :0
idrFrameInterval:30
mvSADoutFlag :0
resetHDVICPeveryFrame:0
enableROI :0
metaDataGenerateConsume:0
maxBitrateCVBR :0
interlaceRefMode:0
enableGDR :0
GDRduration:0
GDRinterval:0
LongTermRefreshInterval:0
UseLongTermFrame:0
SetLongTermFrame:0
VUI_Buffer->timingInfoPresentFlag:1
VUI_Buffer->timeScale :7200
VUI_Buffer->numUnitsInTicks :120
CustomScaleMatrix_Buffer:0x0
CVBRsensitivity:0
CVBRminbitrate :0
LBRmaxpicsize :0
LBRminpicsize :0
LBRskipcontrol :0
maxHighCmpxIntCVBR :0
disableMVDCostFactor:0
putDataGetSpaceFxn :0x0
dataSyncHandle :0x0
==============================================
2.
==========ALG_vidEncCreate VIDENC1_Params ===================
size:124
encodingPreset:2
rateControlPreset:5
maxHeight:1088
maxWidth:1920
maxFrameRate:60000
maxBitRate:12000000
dataEndianness:1
maxInterFrameInterval:1
inputChromaFormat:9
inputContentType:0
reconChromaFormat:9
===============================================
=========== ALG_PrintvidEncDynamicParams IH264VENC_DynamicParams ==========
sliceSize:68
airRate :0
intraFrameQP :28
interPFrameQP:28
initQ :28
rcQMax :51
rcQMin :1
rcQMaxI:51
rcQMinI:1
rcAlgo :1
maxDelay:2000
aspectRatioX:1
aspectRatioY:1
lfDisableIdc:0
enableBufSEI:1
enablePicTimSEI:1
perceptualRC :1
idrFrameInterval:30
mvSADoutFlag :0
resetHDVICPeveryFrame:0
enableROI :1
metaDataGenerateConsume:0
maxBitrateCVBR :0
interlaceRefMode:0
enableGDR :0
GDRduration:0
GDRinterval:0
LongTermRefreshInterval:0
UseLongTermFrame:0
SetLongTermFrame:0
VUI_Buffer->timingInfoPresentFlag:1
VUI_Buffer->timeScale :7200
VUI_Buffer->numUnitsInTicks :120
CustomScaleMatrix_Buffer:0x0
CVBRsensitivity:0
CVBRminbitrate :0
LBRmaxpicsize :0
LBRminpicsize :0
LBRskipcontrol :327684
maxHighCmpxIntCVBR :0
disableMVDCostFactor:0
putDataGetSpaceFxn :0x0
dataSyncHandle :0x0
==============================================