This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Linux boot failed

Part Number: TDA4VM


Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initializatio[ 5.544132] random: crng init done
n.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ 5.592115] CAN device driver interface
[ OK ] Started Daily rotation of log files.
[ OK ] Reached target Timer Units.[ 5.616862] mc: Linux media interface: v0.10

[ 5.617069] cdns-mipi-dphy: probe of 4580000.phy failed with error -2
[ OK ] Listening on Avahi mDNS/DNS-SD Stac[ 5.635600] cdns-mipi-dphy: probe of 4590000.phy failed with error -2
k Activation Socket.
[ 5.663817] videodev: Linux video capture interface: v2.00
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting Weston socket...
[ 5.752741] PVR_K: 188: Device: 4e20000000.gpu
Starting Console System Startup Logging...
Starting D-Bus System Message Bus...
[ 5.820482] SError Interrupt on CPU1, code 0x00000000bf000000 -- SError
[ 5.820501] CPU: 1 PID: 188 Comm: systemd-udevd Tainted: G O 6.1.46-g5892b80d6b #1
[ 5.820506] Hardware name: Texas Instruments K3 J721E SoC (DT)
[ 5.820508] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 5.820512] pc : _RGXReadBVNCFromReg.isra.0+0x20/0x140 [pvrsrvkm]
[ 5.820623] lr : RGXBvncInitialiseConfiguration+0x294/0x980 [pvrsrvkm]
[ 5.820695] sp : ffff800009d0b750
[ 5.820697] x29: ffff800009d0b780 x28: 0000000000000000 x27: 0000000000000000
[ 5.820704] x26: ffff800009d0b758 x25: ffff00084cb68000 x24: ffff00084ca2f1b8
[ 5.820708] x23: 0000000000000000 x22: ffff800000fd8000 x21: ffff00084ca2f008
[ 5.820712] x20: ffff800000f839b8 x19: 0000000000000000 x18: ffff800000f38cb4
[ 5.820716] x17: 000000ffc0000000 x16: ffff800000f39030 x15: ffff800000f38ca0
[ 5.820720] x14: ffff800000f36bf0 x13: ffff800000f42740 x12: ffff800008000000
[ 5.820724] x11: ffff00084ca2f008 x10: 0000000000000020 x9 : 0000000000000000
[ 5.820728] x8 : 0000000000000024 x7 : 0000000000000000 x6 : ffff80000ad80000
[ 5.820732] x5 : ffff800009d0b760 x4 : ffff800009d0b75c x3 : ffff800009d0b758
[ 5.820735] x2 : ffff800009d0b754 x1 : 0000000000000000 x0 : ffff00084ca2f008
[ 5.820741] Kernel panic - not syncing: Asynchronous SError Interrupt
[ 5.820744] CPU: 1 PID: 188 Comm: systemd-udevd Tainted: G O 6.1.46-g5892b80d6b #1
[ 5.820747] Hardware name: Texas Instruments K3 J721E SoC (DT)
[ 5.820749] Call trace:
[ 5.820751] dump_backtrace.part.0+0xdc/0xf0
[ 5.820764] show_stack+0x18/0x30
[ 5.820769] dump_stack_lvl+0x68/0x84
[ 5.820775] dump_stack+0x18/0x34
[ 5.820777] panic+0x188/0x348
[ 5.820783] nmi_panic+0xac/0xb0
[ 5.820790] arm64_serror_panic+0x6c/0x7c
[ 5.820793] do_serror+0x58/0x5c
[ 5.820795] el1h_64_error_handler+0x30/0x4c
[ 5.820799] el1h_64_error+0x64/0x68
[ 5.820802] _RGXReadBVNCFromReg.isra.0+0x20/0x140 [pvrsrvkm]
[ 5.820876] RGXRegisterDevice+0x3c8/0xc00 [pvrsrvkm]
[ 5.820947] PVRSRVCommonDeviceCreate+0x25c/0x750 [pvrsrvkm]
[ 5.821018] pvr_drm_load+0x98/0x1b0 [pvrsrvkm]
[ 5.821087] pvr_probe+0x58/0xbc [pvrsrvkm]
[ 5.821156] platform_probe+0x68/0xe0
[ 5.821161] really_probe+0xbc/0x2dc
[ 5.821167] __driver_probe_device+0x78/0x114
[ 5.821172] driver_probe_device+0xd8/0x15c
[ 5.821175] __driver_attach+0x94/0x19c
[ 5.821180] bus_for_each_dev+0x74/0xd4
[ 5.821184] driver_attach+0x24/0x30
[ 5.821187] bus_add_driver+0x154/0x20c
[ 5.821191] driver_register+0x78/0x130
[ 5.821196] __platform_driver_register+0x28/0x34
[ 5.821198] pvr_init+0x54/0x1000 [pvrsrvkm]
[ 5.821269] do_one_initcall+0x54/0x1d0
[ 5.821272] do_init_module+0x48/0x1d0
[ 5.821278] load_module+0x18f4/0x1c80
[ 5.821282] __do_sys_finit_module+0xac/0x104
[ 5.821287] __arm64_sys_finit_module+0x20/0x30
[ 5.821291] invoke_syscall+0x48/0x114
[ 5.821297] el0_svc_common.constprop.0+0xd4/0xfc
[ 5.821301] do_el0_svc+0x30/0xd0
[ 5.821304] el0_svc+0x2c/0x84
[ 5.821308] el0t_64_sync_handler+0xbc/0x140
[ 5.821311] el0t_64_sync+0x18c/0x190
[ 5.821315] SMP: stopping secondary CPUs
[ 5.821324] Kernel Offset: disabled
[ 5.821325] CPU features: 0x40000,20028084,0000420b
[ 5.821328] Memory Limit: none
[ 6.122540] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---

  • [ 5.820802] _RGXReadBVNCFromReg.isra.0+0x20/0x140 [pvrsrvkm]
    [ 5.820876] RGXRegisterDevice+0x3c8/0xc00 [pvrsrvkm]
    [ 5.820947] PVRSRVCommonDeviceCreate+0x25c/0x750 [pvrsrvkm]
    [ 5.821018] pvr_drm_load+0x98/0x1b0 [pvrsrvkm]
    [ 5.821087] pvr_probe+0x58/0xbc [pvrsrvkm]
    [ 5.821156] platform_probe+0x68/0xe0
    [ 5.821161] really_probe+0xbc/0x2dc
    [ 5.821167] __driver_probe_device+0x78/0x114
    [ 5.821172] driver_probe_device+0xd8/0x15c
    [ 5.821175] __driver_attach+0x94/0x19c
    [ 5.821180] bus_for_each_dev+0x74/0xd4
    [ 5.821184] driver_attach+0x24/0x30
    [ 5.821187] bus_add_driver+0x154/0x20c
    [ 5.821191] driver_register+0x78/0x130
    [ 5.821196] __platform_driver_register+0x28/0x34
    [ 5.821198] pvr_init+0x54/0x1000 [pvrsrvkm]
    [ 5.821269] do_one_initcall+0x54/0x1d0
    [ 5.821272] do_init_module+0x48/0x1d0
    [ 5.821278] load_module+0x18f4/0x1c80
    [ 5.821282] __do_sys_finit_module+0xac/0x104
    [ 5.821287] __arm64_sys_finit_module+0x20/0x30
    [ 5.821291] invoke_syscall+0x48/0x114
    [ 5.821297] el0_svc_common.constprop.0+0xd4/0xfc
    [ 5.821301] do_el0_svc+0x30/0xd0
    [ 5.821304] el0_svc+0x2c/0x84
    [ 5.821308] el0t_64_sync_handler+0xbc/0x140
    [ 5.821311] el0t_64_sync+0x18c/0x190
    [ 5.821315] SMP: stopping secondary CPUs
    [ 5.821324] Kernel Offset: disabled
    [ 5.821325] CPU features: 0x40000,20028084,0000420b
    [ 5.821328] Memory Limit: none
    [ 6.122540] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---

    Hello,

    This is stopping in the GPU kernel driver. Can you please provide the following details:

    1) Which board are you using? Our TDA4VM EVM or a custom board?

    2) Which SDK version are you using? How did you create your setup?

    Regards,

    Erick