C55xx: Can't enable RTDX as it requires AU1 which is already claimed for profiling or breakpoint(s) C55xx: Error: Error 0xA0010002/-1143 Error during: Memory, RTDX, The memory at 0x00000400 continually indicated it was 'not ready' All memory operations currently in progress were aborted in order to regain control of the processor. This is considered a catastrophic event, but the debugger should still be able to access memory and CPU registers. System state has been altered. It is strongly advised that the processor should be reset before resuming execution, My application involves using uart polled mode to get data from a camera and storing it in a sd card using dma mode. Despite the error the program runs fine on execution. Is the board at risk if i use it for my application ? Regards, Rupesh Mehta