Part Number: SK-AM62
Other Parts Discussed in Thread: AM625
Hello! I am creating a serial communication code with the PRU of the AM625, however, despite the flags signaling the reception and transmission of content, because the whiles break, I cannot see the value that I transmit in tx in rx.
I'm using code composer studio and the functions below are just HAL abstractions for the register set:
Can you help me identify the problem?
#include <stdint.h>
#include <pru_uart.c>
#include <pru_gpio.c>
#include <string.h>
#define TX_PIN_ADDRESS ( *( volatile uint32_t * )( 0x000F41DC ) )
#define RX_PIN_ADDRESS ( *( volatile uint32_t * )( 0x000F41D8 ) )
int main(void)
{
char *hostBuffer = "ABC";
volatile uint16_t error = 0;
volatile uint8_t tx = 0;
volatile uint8_t rx = 0;
volatile uint8_t cnt = 0;
TX_PIN_ADDRESS &=~ 0b111;
TX_PIN_ADDRESS |= 0b110;
RX_PIN_ADDRESS &=~ 0b111;
RX_PIN_ADDRESS |= 0b110;
int status_baud = PRU_UART_baudConfig(OVERSAMPLE_16, BAUD_115200);
uint32_t LSB = REG_UART_DIVLSB;
uint32_t MSB = REG_UART_DIVMSB;
int status_lenght = PRU_UART_lenghtConfig(LENGHT_8BITS);
int status_parity = PRU_UART_parityConfig(NO_PARITY);
int status_stop = PRU_UART_stopBitConfig(STOP_BIT);
uint32_t LCR = REG_UART_LCTR;
int status_interrupt_0 = PRU_UART_setInterrupt(TRANSMITTER_HOLDING_EMPTY, UART_INT_ABLE);
int status_interrupt_1 = PRU_UART_setInterrupt(RECIEVER_DATA, UART_INT_DISABLE);
int status_interrupt_2 = PRU_UART_setInterrupt(RECEIVER_LINE_STATUS, UART_INT_DISABLE);
uint32_t inter = REG_UART_INT_EN;
int status_clock_tx = PRU_UART_activateClock(UART_TX, UART_CLK_ABLE);
int status_clock_rx = PRU_UART_activateClock(UART_RX, UART_CLK_ABLE);
int status_fifo = PRU_UART_fifoConfig(UART_FIFO_ABLE);
uint32_t fifo = REG_UART_INT_FIFO;
UART->MCTR_BIT.LOOP = 1;
UART->INT_FIFO_BIT.FCR_RXCLR = 1;
UART->INT_FIFO_BIT.FCR_TXCLR = 1;
while (1)
{
cnt = 0;
while(1)
{
error = PRU_UART_errorCheck( );
if ((tx = hostBuffer[cnt]) == '\0') break;
cnt++;
while ( !UART->LSR1_BIT.TEMT );
UART->RBR_TBR_BIT.TBR_DATA = tx;
error = PRU_UART_errorCheck( );
while ( !UART->LSR1_BIT.DR );
rx = UART->RBR_TBR_BIT.RBR_DATA;
error = PRU_UART_errorCheck( );
}
}
}