This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625-Q1: Can we support Uart use 100MHz?

Part Number: AM625-Q1

Hi Expert,

as you know, our Uart is using 192MHz, but customer want use 100MHz, because they want generate 3.125MHz clock. can we support it?

BR,

Biao 

  • Hello Biao,

    Thanks for your question.

    From the question description I want to clarify few things properly before moving forward.

    I am going to ask in context of UART.



    Based on the above snippet, can tell me the exact numbers the customer is setting up, so that I can look at the support capacity for this and let you know.

    Regards,

    Vaibhav