Other Parts Discussed in Thread: TPS65223
Hi TI team,
Our TDA4V ENTRY design plans to use the PDN-5L solution. I would like to know what the complete order code of the PMIC?
I see that TPS6522311RAHRQ1 is listed in the EVM BOM. The TPS65223 or TPS65221 are mentioned in the J7 SoC power solution. From the draft datasheet of PMIC. I can see that GPIO4 and GPIO5 of 223 have ADC-IN function, but this function is not used in the actual design. So I understand that TPS65221 is ok.
Secondly, I understand that 11 in TPS6522311RAHRQ1 should be the NVM version of PMIC, so should we use 11?
We need to confirm the complete order code as soon as possible for business procurement. Thank you.
Best Regards
Juanli Zhang