Hallo, i've been trying to connect my dm6467t via tftp to a server (Ubuntu) that im using on VMWare on a host WindowsXP machine, i have installed dhcp3 server , also tftpd-hpa, and nfs exports on Ubuntu, but as far as i know, i need to configure dhcp to make the other two protocols run smootly, because im using dinamic ip to connect to the EVM, how can i configure this, ive seen some tutorials on the net, but not a single how to do it for the dm6467t, anyone knows, or know of a page where they say it????
auf wiedersehen, Alan