Part Number: AM6442
On TI RPMsg Char Package using Ubuntu 22.04 LTS
under build
1) ARM has changed the way they bundled cross-compiler tools; see https://learn.arm.com/install-guides/gcc/cross/ 21Dec2023 (cannot get at "gcc-arm-9.2-2019.12*" explicitly)
Is it safe to use the installs as ARM prescribes for Ubuntu packages being installed, i.e.
"
Installing on Debian based distributions such as Ubuntu
Use the apt command to install software packages on any Debian based Linux distribution.
sudo apt update
sudo apt install gcc-arm-none-eabi -y
sudo apt install gcc-arm-linux-gnueabihf -y
sudo apt install gcc-aarch64-linux-gnu -y
"
2) On the GNU tools, one may need to install m4 before one installs autoconf.
I am slated to use
autoconf 2.7102
automake 1.16.5-1.3
libtool 2,4,6-15 build 2
IS there some risk in using this combination?