This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About AM35x GPMC syncronous(gpmc_clk) speed

Guru 10570 points

Hello.

There are two descriptions about GPMC speed in AM35x datasheet.

SPRS550c
 a) (P1) Memory Interfaces:
    Up to 83 MHz General Purpose Memory Interface supporting 16-bit Wide

 b) (P108) Table 6-4. GPMC/NOR Flash Interface Switching Characteristics Synchronous Mode
    F0 tc(CLK) .. Cycle time, output clock gpmc_clk .. 10 ns[MIN]

Question)
 - Which one is the correct about gpmc_clk ?
 - Is incorrect description just a mistake?

Best regards,
RY