This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515 FDK Flexibility



Hi, I am about to buy a Fingerprint Development Kit . I want to develop a project in where I send some fingerprint data across a bluetooth transceiver I wonder if the FDK allow me to easily interconnect the transceiver with the DSP and modify the code in order to send it. If not  I need it for an important project.  Please help.

  • The FDK kit itself does not include the BlueTooth transceiver. However, the FDK kit is consist of two boards, one the extension board, the other is the core board which has the C5515 on it, and the fingerprint processing is done by the C5515. We open the interface between the core board and extension board. The solution is: you can build yourown extension board with the same interface, but add the Bluetooth transceiver on the your extension board.

    Regards

    Wen