Hi guys,
in our board, based on DM368 device, we are trying to write the NOR flash (S29GL128N/P) using the sfh_DM36x.exe flash tool. The serial output of the software sfh_DM36x.exe gives the error "Addressing error" when it tries to erase the flash and therefore we can't flash the NOR with the UBL and the u-boot. But, if we use the XDS100 development tool we can write the NOR and we are also able to start the kernel; in this situation we think that the hardware could be right. Our suspicion is that the SFT downloaded from the sfh_DM36x.exe isn't correct or that there is another version of the software only for the NOR. May be?
Could you please help us to solve the serial flashing problem?
Thank you.
Loris