good day
And I have two examples here with me is exactly what
I need more I can not
put the two together.
Will I have any that could put them together
for me and the audio with priority over the
network.
Examples
are helloWord in
this directory file:///C:/CCStudio_v3.3/ndk_2_0_0/packages/ti/ndk/example/network/helloWorld/evm6747
and the other in the directory file:///C:/Program%20Files/Texas%20Instruments/pspdrivers_01_20_00/packages/ti/pspiom/examples/evm6747/audio/
I would like if possible to do both become possible only if a program can send me e-mail Leandro_nando84@Hotmail.com.