Part Number: AM62A3
Hi all,
a customer is designing with the AM62A3 device.
there is a question about the skew in Table 2-7 in the AM62A LPDDR4 guidelines specifically LP4_DRS5 at 150ps.
The spec below mentioned the mismatch between DQ & DQS (LP4_DRS6) can be up to -49ps. For a 4Gbps data rate, this translates to -19.6% of the UI. Could you clarify if this value is within the expected range for LPDDR4 tolerance?
And for LP4_DRS5, if we adhere to the maximum skew of up to 150ps, the flight time difference of data bytes translates to 60% of the UI @4Gbps data rate, any concern on potential training failure or other performance issue associated with such skew level? Pls advise.
The 150ps seems very high.

In comparison the LPDDR4 guideline for AM64xx shows in Table 3-7 LP4_DRS4 and LP4_DRS5 at 2ps.
https://www.ti.com/lit/an/spracu1a/spracu1a.pdf
Is there an issue in the AM62A Table 2-7 for these values above?

Thanks!
--Gunter