This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721S2XSOMXEVM: PSDK RTOS: TIDL OD with camera application overlay issue with no object name mentioned while detection.

Part Number: J721S2XSOMXEVM


Hello Team,

Board: J721S2 EVM

I am having an issue while running the OD with camera application as the object detection by the TIDL model shows only the boundry box and not the object name in the top.

As per my search, the OD is happening in C7X core and there is no graphics libs included to create a text box for object name to display. Also i am trying to do sensor fusion with RADAR and  Camera object 

data from the application.

I would like to give me a support to get the object detections info to the HLOS so that i can able to perform sensor fusion in the application.

Thanks in advance!!!

Regards,

Dinesh kumar S