we are working on DM816x EVM , i need to run an custom OpenGL Application 'GLmark' which uses libraries such as
- SDML(Simple Direct Media Layer Library which will be used by OpenGL)
- GLEW (OpenGL Extension Wrangler Library(GLEW), a cross-platform C/C++ library that helps in querying and loading OpenGL extensions. )
- MESA(Mesa 3D is an open source 3D computer graphics library that provides a generic OpenGL implementation for rendering three-dimensional graphics on multiple platforms ) and
- libxmu (a library for programming on the X Window System )
the application is complied with above libraries and exported the binaries and libraries to the target EVM and when i ran this the binaries it throws an error stating "[ Fail ] - Video mode set failed: No video mode large enough for 800x600 Segmentation fault", when i checked this error it gives me indication that SDML library was not able to create an graphics window with given resolution . i checked with so many resolutions like 1024 x 768 it gives same error . this application is used for running on systems which has X Window systems support in it ( basically on desktop PC's which has operating system in it
my question is whether can i run this kind of custom OpenGL app in the DM816x Target EVM which requires Xwindow system support ? or in order to run this app on Dm816x what are the things i need to take care w.r.t Opengl support , graphics support?
i had went through so many documents like DM816x_C6A816x_AM389x_EZ_Software_Developers_Guide.pdf, PSP document (http://processors.wiki.ti.com/index.php/DM816x_C6A816x_AM389x_PSP_User_Guide)
but none of this were able to give me some direction for my issue. request your help on this regards
--chethan