This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x: EZSDK 5.02.01.59 and linux kernel commit ID from arago

Hi,

 

I wanted to make sure how the kernel in the latest EZSDK .59 was created. Here is what I am thinking:

(1) Go to http://www.arago-project.org/git/projects/?p=linux-omap3.git;a=shortlog;h=refs/heads/ti81xx-master

(2) Use tag http://www.arago-project.org/git/projects/?p=linux-omap3.git;a=commit;h=17b514af7d584677e071d488a3be011ad3078038

(3) Then apply two more patches from the quilt directory /patches in the SDK .59

 

Is this correct?

 

Another question: How much has the ti81xx-master been merged into the master branch?

 

Thanks,

--Gunter