This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C66x - GbE MAC configuration

Guru 10750 points

Hi,

- According to sprugv9a (p#72) the address of port "0" MAC_MAC_CTL is 904h and port "1" MAC_MAC_CTL is A04h but what I have seen is that the actual address of port "1" MAC_MAC_CTL is 944h, is this correct?

- There are some statistics registers which are not defined - I'm running eth. project and I'm getting statistics at address "0xC34, 0xC38, 0xC64 and 0xC74" what are these addresses represent's?

Thanks,

HR