hello
Based on sdk9.1, we want to print buf in tensors and have modified the following code:
the code in the c7x-mma-tidl/arm-tidl/tiovx_kernels/tidl/dsp/vx_tidl_target.c file
Output the following error:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Yang,
It is our pleasure to help.
There should be a few lines at the bottom of the core dump that give a bit more indication of the type of error that happened. Would you please share that?
It is not clear why the tensor_counter is jumping directly from 319 to 1019.
Best regards,
Qutaiba
hello
this is c7X file log
root@am62axx-evm:/opt/edgeai-gst-apps# /opt/vision_apps/vx_app_arm_remote_log.out [MCU1_0] 68362.210908 s: CIO: Init ... Done !!! [MCU1_0] 68362.210950 s: APP: Init ... !!! [MCU1_0] 68362.210979 s: MEM: Init ... !!! [MCU1_0] 68362.210996 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ af000000 of size 16777216 bytes !!! [MCU1_0] 68362.211035 s: MEM: Init ... Done !!! [MCU1_0] 68362.211062 s: IPC: Init ... !!! [MCU1_0] 68362.211080 s: IPC: 3 CPUs participating in IPC !!! [MCU1_0] 68362.211375 s: IPC: Waiting for HLOS to be ready ... !!! [MCU1_0] 68362.215726 s: #Sciserver Version: v2023.11.0.0REL.MCUSDK.MM.NN.PP.bb [MCU1_0] 68362.218500 s: ##RM_PM_HAL Version: vMM.NN.PP [MCU1_0] 68362.221447 s: ##Starting Sciserver..... PASSED [MCU1_0] 68374.022665 s: IPC: HLOS is ready !!! [MCU1_0] 68374.022804 s: IPC: Init ... Done !!! [MCU1_0] 68374.022830 s: APP: Syncing with 2 CPUs ... !!! [MCU1_0] 68374.078329 s: APP: Syncing with 2 CPUs ... Done !!! [MCU1_0] 68374.078365 s: REMOTE_SERVICE: Init ... !!! [MCU1_0] 68374.078592 s: REMOTE_SERVICE: Init ... Done !!! [MCU1_0] 68374.078618 s: FVID2: Init ... !!! [MCU1_0] 68374.078646 s: FVID2: Init ... Done !!! [MCU1_0] 68374.078663 s: VHWA: VPAC Init ... !!! [MCU1_0] 68374.078678 s: SCICLIENT: Sciclient_pmSetModuleState module=219 state=2 [MCU1_0] 68374.078759 s: SCICLIENT: Sciclient_pmSetModuleState success [MCU1_0] 68374.078783 s: VHWA: LDC Init ... !!! [MCU1_0] 68374.078875 s: VHWA: LDC Init ... Done !!! [MCU1_0] 68374.078899 s: VHWA: MSC Init ... !!! [MCU1_0] 68374.079321 s: VHWA: MSC Init ... Done !!! [MCU1_0] 68374.079342 s: VHWA: VISS Init ... !!! [MCU1_0] 68374.079466 s: VHWA: VISS Init ... Done !!! [MCU1_0] 68374.079486 s: VHWA: VPAC Init ... Done !!! [MCU1_0] 68374.079510 s: VX_ZONE_INIT:Enabled [MCU1_0] 68374.079528 s: VX_ZONE_ERROR:Enabled [MCU1_0] 68374.079549 s: VX_ZONE_WARNING:Enabled [MCU1_0] 68374.080548 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU1-0 [MCU1_0] 68374.080674 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_LDC1 [MCU1_0] 68374.080756 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC1 [MCU1_0] 68374.080833 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC2 [MCU1_0] 68374.080903 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_VISS1 [MCU1_0] 68374.080935 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [MCU1_0] 68374.080995 s: APP: OpenVX Target kernel init ... !!! [MCU1_0] 68374.084927 s: APP: OpenVX Target kernel init ... Done !!! [MCU1_0] 68374.084954 s: VISS REMOTE SERVICE: Init ... !!! [MCU1_0] 68374.084996 s: VISS REMOTE SERVICE: Init ... Done !!! [MCU1_0] 68374.085022 s: APP: Init ... Done !!! [MCU1_0] 68374.085040 s: APP: Run ... !!! [MCU1_0] 68374.085054 s: IPC: Starting echo test ... [MCU1_0] 68374.085328 s: APP: Run ... Done !!! [MCU1_0] 68374.086245 s: IPC: Echo status: a530-0[x] r5f0-0[s] c75ss0[P] [C7x_1 ] 68374.066832 s: CIO: Init ... Done !!! [C7x_1 ] 68374.066851 s: APP: Init ... !!! [C7x_1 ] 68374.066865 s: SCICLIENT: Init ... !!! [C7x_1 ] 68374.066929 s: SCICLIENT: DMSC FW version [9.1.8--v09.01.08 (Kool Koala)] [C7x_1 ] 68374.066948 s: SCICLIENT: DMSC FW revision 0x9 [C7x_1 ] 68374.066961 s: SCICLIENT: DMSC FW ABI revision 3.1 [C7x_1 ] 68374.066976 s: SCICLIENT: Init ... Done !!! [C7x_1 ] 68374.066989 s: UDMA: Init ... !!! [C7x_1 ] 68374.067001 s: UDMA: Init ... Done !!! [C7x_1 ] 68374.067013 s: MEM: Init ... !!! [C7x_1 ] 68374.067026 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ b2000000 of size 117440512 bytes !!! [C7x_1 ] 68374.067054 s: MEM: Init ... Done !!! [C7x_1 ] 68374.067066 s: IPC: Init ... !!! [C7x_1 ] 68374.067078 s: IPC: 3 CPUs participating in IPC !!! [C7x_1 ] 68374.067309 s: IPC: Waiting for HLOS to be ready ... !!! [C7x_1 ] 68374.078206 s: IPC: HLOS is ready !!! [C7x_1 ] 68374.078299 s: IPC: Init ... Done !!! [C7x_1 ] 68374.078313 s: APP: Syncing with 2 CPUs ... !!! [C7x_1 ] 68374.078328 s: APP: Syncing with 2 CPUs ... Done !!! [C7x_1 ] 68374.078342 s: REMOTE_SERVICE: Init ... !!! [C7x_1 ] 68374.079254 s: REMOTE_SERVICE: Init ... Done !!! [C7x_1 ] 68374.079279 s: VX_ZONE_INIT:Enabled [C7x_1 ] 68374.079294 s: VX_ZONE_ERROR:Enabled [C7x_1 ] 68374.079306 s: VX_ZONE_WARNING:Enabled [C7x_1 ] 68374.079983 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1 [C7x_1 ] 68374.080076 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_2 [C7x_1 ] 68374.080173 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_3 [C7x_1 ] 68374.080263 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_4 [C7x_1 ] 68374.080351 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_5 [C7x_1 ] 68374.080441 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_6 [C7x_1 ] 68374.080534 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_7 [C7x_1 ] 68374.080624 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:59] Added target DSP_C7-1_PRI_8 [C7x_1 ] 68374.080654 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! [C7x_1 ] 68374.080671 s: APP: OpenVX Target kernel init ... !!! [C7x_1 ] 68374.080887 s: APP: OpenVX Target kernel init ... Done !!! [C7x_1 ] 68374.080902 s: APP: Init ... Done !!! [C7x_1 ] 68374.080915 s: APP: Run ... !!! [C7x_1 ] 68374.080926 s: IPC: Starting echo test ... [C7x_1 ] 68374.081084 s: APP: Run ... Done !!! [C7x_1 ] 68374.086317 s: IPC: Echo status: a530-0[x] r5f0-0[P] c75ss0[s] [C7x_1 ] 68721.834799 s: PREEMPTION: Requesting memory of size 1048576 for targetPriority = 0 [C7x_1 ] 68721.834827 s: [C7x_1 ] 68721.834848 s: -------------------------------------------- [C7x_1 ] 68721.834876 s: TIDL Memory size requiement (record wise): [C7x_1 ] 68721.834922 s: MemRecNum , Space , Attribute , Alignment , Size(KBytes), BasePtr [C7x_1 ] 68721.834985 s: 0 , DDR Cacheable , Persistent , 128, 15.25 , 0x00000000 [C7x_1 ] 68721.835036 s: 1 , DDR Cacheable , Persistent , 128, 0.64 , 0x00000000 [C7x_1 ] 68721.835084 s: 2 , L1D , Scratch , 128, 16.00 , 0x00000000 [C7x_1 ] 68721.835134 s: 3 , L2 , Scratch , 128, 224.00 , 0x00000000 [C7x_1 ] 68721.835183 s: 4 , L3/MSMC , Scratch , 128, 1024.00 , 0x00000000 [C7x_1 ] 68721.835231 s: 5 , DDR Cacheable , Persistent , 128, 11598.62, 0x00000000 [C7x_1 ] 68721.835279 s: 6 , DDR Cacheable , Scratch , 128, 15.75 , 0x00000000 [C7x_1 ] 68721.835328 s: 7 , DDR Cacheable , Persistent , 128, 4947.75 , 0x00000000 [C7x_1 ] 68721.835376 s: 8 , DDR Cacheable , Scratch , 128, 0.13 , 0x00000000 [C7x_1 ] 68721.835424 s: 9 , DDR Cacheable , Scratch , 128, 3.13 , 0x00000000 [C7x_1 ] 68721.835473 s: 10 , DDR Cacheable , Persistent , 128, 1335.34 , 0x00000000 [C7x_1 ] 68721.835522 s: 11 , DDR Cacheable , Scratch , 128, 512.25 , 0x00000000 [C7x_1 ] 68721.835571 s: 12 , DDR Cacheable , Persistent , 128, 1024.00 , 0x00000000 [C7x_1 ] 68721.835620 s: 13 , DDR Cacheable , Persistent , 128, 2165.46 , 0x00000000 [C7x_1 ] 68721.835667 s: 14 , DDR Cacheable , Persistent , 128, 0.14 , 0x00000000 [C7x_1 ] 68721.835702 s: -------------------------------------------- [C7x_1 ] 68721.835731 s: Total memory size requirement (space wise): [C7x_1 ] 68721.835754 s: Mem Space , Size(KBytes) [C7x_1 ] 68721.835777 s: L1D , 16.00 [C7x_1 ] 68721.835801 s: L2 , 224.00 [C7x_1 ] 68721.835824 s: L3/MSMC , 1024.00 [C7x_1 ] 68721.835847 s: DDR Cacheable, 21618.46 [C7x_1 ] 68721.835875 s: -------------------------------------------- [C7x_1 ] 68721.835914 s: NOTE: Memory requirement in host emulation can be different from the same on EVM [C7x_1 ] 68721.835963 s: To get the actual TIDL memory requirement make sure to run on EVM with [C7x_1 ] 68721.835992 s: debugTraceLevel = 2 [C7x_1 ] 68721.836003 s: [C7x_1 ] 68721.836024 s: -------------------------------------------- [C7x_1 ] 68721.837267 s: TIDL init call from ivision API [C7x_1 ] 68721.837287 s: [C7x_1 ] 68721.837306 s: -------------------------------------------- [C7x_1 ] 68721.837334 s: TIDL Memory size requiement (record wise): [C7x_1 ] 68721.837376 s: MemRecNum , Space , Attribute , Alignment , Size(KBytes), BasePtr [C7x_1 ] 68721.837426 s: 0 , DDR Cacheable , Persistent , 128, 15.25 , 0xb200fc40 [C7x_1 ] 68721.837474 s: 1 , DDR Cacheable , Persistent , 128, 0.64 , 0xb2013980 [C7x_1 ] 68721.837524 s: 2 , L1D , Scratch , 128, 16.00 , 0x7f03c000 [C7x_1 ] 68721.837572 s: 3 , L2 , Scratch , 128, 224.00 , 0x7f000000 [C7x_1 ] 68721.837621 s: 4 , L3/MSMC , Scratch , 128, 1024.00 , 0x7e000000 [C7x_1 ] 68721.837670 s: 5 , DDR Cacheable , Persistent , 128, 11598.62, 0xb2013cc0 [C7x_1 ] 68721.837718 s: 6 , DDR Cacheable , Scratch , 128, 15.75 , 0xb9000000 [C7x_1 ] 68721.837766 s: 7 , DDR Cacheable , Persistent , 128, 4947.75 , 0xb2b67780 [C7x_1 ] 68721.837813 s: 8 , DDR Cacheable , Scratch , 128, 0.13 , 0xb9004000 [C7x_1 ] 68721.837862 s: 9 , DDR Cacheable , Scratch , 128, 3.13 , 0xb9004400 [C7x_1 ] 68721.837910 s: 10 , DDR Cacheable , Persistent , 128, 1335.34 , 0xb303c6c0 [C7x_1 ] 68721.837964 s: 11 , DDR Cacheable , Scratch , 128, 512.25 , 0xb9005400 [C7x_1 ] 68721.838015 s: 12 , DDR Cacheable , Persistent , 128, 1024.00 , 0xb318a480 [C7x_1 ] 68721.838064 s: 13 , DDR Cacheable , Persistent , 128, 2165.46 , 0xb328a4c0 [C7x_1 ] 68721.838112 s: 14 , DDR Cacheable , Persistent , 128, 0.14 , 0xb34a7b00 [C7x_1 ] 68721.838146 s: -------------------------------------------- [C7x_1 ] 68721.838175 s: Total memory size requirement (space wise): [C7x_1 ] 68721.838197 s: Mem Space , Size(KBytes) [C7x_1 ] 68721.838219 s: L1D , 16.00 [C7x_1 ] 68721.838243 s: L2 , 224.00 [C7x_1 ] 68721.838265 s: L3/MSMC , 1024.00 [C7x_1 ] 68721.838288 s: DDR Cacheable, 21618.46 [C7x_1 ] 68721.838315 s: -------------------------------------------- [C7x_1 ] 68721.838354 s: NOTE: Memory requirement in host emulation can be different from the same on EVM [C7x_1 ] 68721.838395 s: To get the actual TIDL memory requirement make sure to run on EVM with [C7x_1 ] 68721.838421 s: debugTraceLevel = 2 [C7x_1 ] 68721.838432 s: [C7x_1 ] 68721.838453 s: -------------------------------------------- [C7x_1 ] 68721.846131 s: Alg Init for Layer # - 1 [C7x_1 ] 68721.846388 s: Alg Init for Layer # - 2 [C7x_1 ] 68721.846920 s: Alg Init for Layer # - 3 [C7x_1 ] 68721.847157 s: Alg Init for Layer # - 4 [C7x_1 ] 68721.847393 s: Alg Init for Layer # - 5 [C7x_1 ] 68721.847614 s: Alg Init for Layer # - 6 [C7x_1 ] 68721.847856 s: Alg Init for Layer # - 7 [C7x_1 ] 68721.848043 s: Alg Init for Layer # - 8 [C7x_1 ] 68721.848223 s: Alg Init for Layer # - 9 [C7x_1 ] 68721.848462 s: Alg Init for Layer # - 10 [C7x_1 ] 68721.848922 s: Alg Init for Layer # - 11 [C7x_1 ] 68721.849183 s: Alg Init for Layer # - 13 [C7x_1 ] 68721.849399 s: Alg Init for Layer # - 14 [C7x_1 ] 68721.849700 s: Alg Init for Layer # - 15 [C7x_1 ] 68721.849890 s: Alg Init for Layer # - 16 [C7x_1 ] 68721.850110 s: Alg Init for Layer # - 17 [C7x_1 ] 68721.850411 s: Alg Init for Layer # - 18 [C7x_1 ] 68721.850598 s: Alg Init for Layer # - 12 [C7x_1 ] 68721.850819 s: Alg Init for Layer # - 19 [C7x_1 ] 68721.851011 s: Alg Init for Layer # - 20 [C7x_1 ] 68721.851255 s: Alg Init for Layer # - 21 [C7x_1 ] 68721.852223 s: Alg Init for Layer # - 22 [C7x_1 ] 68721.852533 s: Alg Init for Layer # - 24 [C7x_1 ] 68721.852796 s: Alg Init for Layer # - 25 [C7x_1 ] 68721.853378 s: Alg Init for Layer # - 26 [C7x_1 ] 68721.853567 s: Alg Init for Layer # - 27 [C7x_1 ] 68721.853821 s: Alg Init for Layer # - 28 [C7x_1 ] 68721.854397 s: Alg Init for Layer # - 29 [C7x_1 ] 68721.854581 s: Alg Init for Layer # - 30 [C7x_1 ] 68721.854834 s: Alg Init for Layer # - 31 [C7x_1 ] 68721.855405 s: Alg Init for Layer # - 32 [C7x_1 ] 68721.855590 s: Alg Init for Layer # - 23 [C7x_1 ] 68721.855877 s: Alg Init for Layer # - 33 [C7x_1 ] 68721.856078 s: Alg Init for Layer # - 34 [C7x_1 ] 68721.856456 s: Alg Init for Layer # - 35 [C7x_1 ] 68721.859379 s: Alg Init for Layer # - 36 [C7x_1 ] 68721.860252 s: Alg Init for Layer # - 37 [C7x_1 ] 68721.860818 s: Alg Init for Layer # - 39 [C7x_1 ] 68721.861228 s: Alg Init for Layer # - 40 [C7x_1 ] 68721.862826 s: Alg Init for Layer # - 38 [C7x_1 ] 68721.863373 s: Alg Init for Layer # - 41 [C7x_1 ] 68721.863577 s: Alg Init for Layer # - 42 [C7x_1 ] 68721.864417 s: Alg Init for Layer # - 43 [C7x_1 ] 68721.864967 s: Alg Init for Layer # - 44 [C7x_1 ] 68721.865139 s: Alg Init for Layer # - 45 [C7x_1 ] 68721.865323 s: Alg Init for Layer # - 46 [C7x_1 ] 68721.865738 s: Alg Init for Layer # - 48 [C7x_1 ] 68721.866038 s: Alg Init for Layer # - 49 [C7x_1 ] 68721.866645 s: Alg Init for Layer # - 50 [C7x_1 ] 68721.866945 s: Alg Init for Layer # - 51 [C7x_1 ] 68721.867561 s: Alg Init for Layer # - 47 [C7x_1 ] 68721.868010 s: Alg Init for Layer # - 52 [C7x_1 ] 68721.868220 s: Alg Init for Layer # - 53 [C7x_1 ] 68721.868648 s: Alg Init for Layer # - 54 [C7x_1 ] 68721.869009 s: Alg Init for Layer # - 55 [C7x_1 ] 68721.869172 s: Alg Init for Layer # - 56 [C7x_1 ] 68721.869361 s: Alg Init for Layer # - 57 [C7x_1 ] 68721.869644 s: Alg Init for Layer # - 59 [C7x_1 ] 68721.869881 s: Alg Init for Layer # - 60 [C7x_1 ] 68721.870213 s: Alg Init for Layer # - 61 [C7x_1 ] 68721.870451 s: Alg Init for Layer # - 62 [C7x_1 ] 68721.870774 s: Alg Init for Layer # - 58 [C7x_1 ] 68721.871102 s: Alg Init for Layer # - 63 [C7x_1 ] 68721.871295 s: Alg Init for Layer # - 64 [C7x_1 ] 68721.871575 s: Alg Init for Layer # - 65 [C7x_1 ] 68721.872249 s: Alg Init for Layer # - 68 [C7x_1 ] 68721.872463 s: Alg Init for Layer # - 69 [C7x_1 ] 68721.872792 s: Alg Init for Layer # - 75 [C7x_1 ] 68721.873094 s: Alg Init for Layer # - 83 [C7x_1 ] 68721.873731 s: Alg Init for Layer # - 85 [C7x_1 ] 68721.874054 s: Alg Init for Layer # - 87 [C7x_1 ] 68721.874689 s: Alg Init for Layer # - 73 [C7x_1 ] 68721.875049 s: Alg Init for Layer # - 88 [C7x_1 ] 68721.875255 s: Alg Init for Layer # - 89 [C7x_1 ] 68721.875699 s: Alg Init for Layer # - 90 [C7x_1 ] 68721.877322 s: Alg Init for Layer # - 94 [C7x_1 ] 68721.877540 s: Alg Init for Layer # - 95 [C7x_1 ] 68721.878117 s: Alg Init for Layer # - 103 [C7x_1 ] 68721.878555 s: Alg Init for Layer # - 119 [C7x_1 ] 68721.880179 s: Alg Init for Layer # - 121 [C7x_1 ] 68721.880600 s: Alg Init for Layer # - 123 [C7x_1 ] 68721.882228 s: Alg Init for Layer # - 101 [C7x_1 ] 68721.882806 s: Alg Init for Layer # - 124 [C7x_1 ] 68721.883047 s: Alg Init for Layer # - 125 [C7x_1 ] 68721.883921 s: Alg Init for Layer # - 126 [C7x_1 ] 68721.884577 s: Alg Init for Layer # - 127 [C7x_1 ] 68721.886608 s: Alg Init for Layer # - 131 [C7x_1 ] 68721.888693 s: Alg Init for Layer # - 138 [C7x_1 ] 68721.889205 s: Alg Init for Layer # - 139 [C7x_1 ] 68721.889513 s: Alg Init for Layer # - 128 [C7x_1 ] 68721.891543 s: Alg Init for Layer # - 132 [C7x_1 ] 68721.891864 s: Alg Init for Layer # - 129 [C7x_1 ] 68721.893890 s: Alg Init for Layer # - 133 [C7x_1 ] 68721.894216 s: Alg Init for Layer # - 130 [C7x_1 ] 68721.896255 s: Alg Init for Layer # - 134 [C7x_1 ] 68721.896582 s: Alg Init for Layer # - 92 [C7x_1 ] 68721.896925 s: Alg Init for Layer # - 99 [C7x_1 ] 68721.897670 s: Alg Init for Layer # - 108 [C7x_1 ] 68721.897972 s: Alg Init for Layer # - 100 [C7x_1 ] 68721.898665 s: Alg Init for Layer # - 110 [C7x_1 ] 68721.898947 s: Alg Init for Layer # - 109 [C7x_1 ] 68721.899227 s: Alg Init for Layer # - 107 [C7x_1 ] 68721.899491 s: Alg Init for Layer # - 91 [C7x_1 ] 68721.899851 s: Alg Init for Layer # - 93 [C7x_1 ] 68721.900589 s: Alg Init for Layer # - 102 [C7x_1 ] 68721.901354 s: Alg Init for Layer # - 118 [C7x_1 ] 68721.901723 s: Alg Init for Layer # - 120 [C7x_1 ] 68721.902039 s: Alg Init for Layer # - 96 [C7x_1 ] 68721.902751 s: Alg Init for Layer # - 104 [C7x_1 ] 68721.903056 s: Alg Init for Layer # - 97 [C7x_1 ] 68721.903775 s: Alg Init for Layer # - 105 [C7x_1 ] 68721.904084 s: Alg Init for Layer # - 98 [C7x_1 ] 68721.904781 s: Alg Init for Layer # - 106 [C7x_1 ] 68721.905090 s: Alg Init for Layer # - 66 [C7x_1 ] 68721.905354 s: Alg Init for Layer # - 67 [C7x_1 ] 68721.905726 s: Alg Init for Layer # - 74 [C7x_1 ] 68721.906120 s: Alg Init for Layer # - 82 [C7x_1 ] 68721.906389 s: Alg Init for Layer # - 84 [C7x_1 ] 68721.906656 s: Alg Init for Layer # - 70 [C7x_1 ] 68721.907084 s: Alg Init for Layer # - 76 [C7x_1 ] 68721.907358 s: Alg Init for Layer # - 71 [C7x_1 ] 68721.907750 s: Alg Init for Layer # - 77 [C7x_1 ] 68721.908037 s: Alg Init for Layer # - 72 [C7x_1 ] 68721.908414 s: Alg Init for Layer # - 78 [C7x_1 ] 68721.908779 s: PREEMPTION: Adding a new priority object for targetPriority = 0, handle = b200fc40 [C7x_1 ] 68721.908845 s: PREEMPTION: Now total number of priority objects = 1 at priorityId = 0, with new memRec of base = b318a480 and size = 1048576 [C7x_1 ] 68721.908911 s: PREEMPTION: Requesting context memory addr for handle b200fc40, return Addr = 99dde450 [C7x_1 ] 68721.908959 s: Print preEmption Hnadle during init stage : [C7x_1 ] 68721.908990 s: Procsize, ctxSize, lyrIdx [C7x_1 ] 68721.909021 s: 0.000, 6632, 0 [C7x_1 ] 68721.909052 s: 0.579, 6632, 1 [C7x_1 ] 68721.909081 s: 0.607, 6632, 2 [C7x_1 ] 68721.909110 s: 0.189, 725352, 3 [C7x_1 ] 68721.909139 s: 0.280, 725352, 4 [C7x_1 ] 68721.909168 s: 0.188, 725352, 5 [C7x_1 ] 68721.909196 s: 0.236, 725352, 6 [C7x_1 ] 68721.909224 s: 0.279, 725352, 7 [C7x_1 ] 68721.909252 s: 0.188, 6632, 8 [C7x_1 ] 68721.909280 s: 0.371, 6632, 9 [C7x_1 ] 68721.909307 s: 0.473, 730728, 10 [C7x_1 ] 68721.909335 s: 0.065, 730728, 11 [C7x_1 ] 68721.909363 s: 0.098, 730728, 12 [C7x_1 ] 68721.909391 s: 0.238, 730728, 13 [C7x_1 ] 68721.909419 s: 0.143, 730728, 14 [C7x_1 ] 68721.909446 s: 0.098, 730728, 15 [C7x_1 ] 68721.909474 s: 0.238, 730728, 16 [C7x_1 ] 68721.909502 s: 0.143, 730728, 17 [C7x_1 ] 68721.909529 s: 0.065, 368744, 18 [C7x_1 ] 68721.909556 s: 0.097, 6632, 19 [C7x_1 ] 68721.909585 s: 0.123, 730728, 20 [C7x_1 ] 68721.909612 s: 0.439, 730728, 21 [C7x_1 ] 68721.909640 s: 0.060, 910056, 22 [C7x_1 ] 68721.909668 s: 0.037, 910056, 23 [C7x_1 ] 68721.909696 s: 0.249, 910056, 24 [C7x_1 ] 68721.909723 s: 0.052, 910056, 25 [C7x_1 ] 68721.909750 s: 0.037, 910056, 26 [C7x_1 ] 68721.909777 s: 0.249, 910056, 27 [C7x_1 ] 68721.909805 s: 0.052, 910056, 28 [C7x_1 ] 68721.909833 s: 0.037, 910056, 29 [C7x_1 ] 68721.909860 s: 0.249, 910056, 30 [C7x_1 ] 68721.909887 s: 0.052, 910056, 31 [C7x_1 ] 68721.909915 s: 0.078, 910056, 32 [C7x_1 ] 68721.909947 s: 0.097, 730728, 33 [C7x_1 ] 68721.909978 s: 0.104, 730728, 34 [C7x_1 ] 68721.910006 s: 0.516, 931560, 35 [C7x_1 ] 68721.910034 s: 0.124, 931560, 36 [C7x_1 ] 68721.910062 s: 0.066, 931560, 37 [C7x_1 ] 68721.910089 s: 0.036, 931560, 38 [C7x_1 ] 68721.910116 s: 0.269, 931560, 39 [C7x_1 ] 68721.910143 s: 0.065, 831208, 40 [C7x_1 ] 68721.910170 s: 0.032, 730728, 41 [C7x_1 ] 68721.910198 s: 0.124, 988904, 42 [C7x_1 ] 68721.910225 s: 0.065, 859880, 43 [C7x_1 ] 68721.910252 s: 0.054, 859880, 44 [C7x_1 ] 68721.910280 s: 0.194, 859880, 45 [C7x_1 ] 68721.910307 s: 0.126, 859880, 46 [C7x_1 ] 68721.910334 s: 0.053, 859880, 47 [C7x_1 ] 68721.910361 s: 0.249, 859880, 48 [C7x_1 ] 68721.910388 s: 0.053, 859880, 49 [C7x_1 ] 68721.910416 s: 0.249, 859880, 50 [C7x_1 ] 68721.910443 s: 0.126, 859880, 51 [C7x_1 ] 68721.910470 s: 0.100, 859880, 52 [C7x_1 ] 68721.910498 s: 0.109, 859880, 53 [C7x_1 ] 68721.910526 s: 0.082, 859880, 54 [C7x_1 ] 68721.910554 s: 0.124, 859880, 55 [C7x_1 ] 68721.910581 s: 0.188, 135784, 56 [C7x_1 ] 68721.910609 s: 0.190, 497896, 57 [C7x_1 ] 68721.910637 s: 0.036, 497896, 58 [C7x_1 ] 68721.910664 s: 0.238, 497896, 59 [C7x_1 ] 68721.910692 s: 0.036, 497896, 60 [C7x_1 ] 68721.910719 s: 0.238, 497896, 61 [C7x_1 ] 68721.910746 s: 0.235, 497896, 62 [C7x_1 ] 68721.910774 s: 0.188, 135784, 63 [C7x_1 ] 68721.910801 s: 0.123, 859880, 64 [C7x_1 ] 68721.910828 s: 0.251, 859880, 65 [C7x_1 ] 68721.910856 s: 0.100, 859880, 66 [C7x_1 ] 68721.910883 s: 0.078, 859880, 67 [C7x_1 ] 68721.910911 s: 0.053, 859880, 68 [C7x_1 ] 68721.910943 s: 0.249, 859880, 69 [C7x_1 ] 68721.910974 s: 0.053, 859880, 70 [C7x_1 ] 68721.911002 s: 0.249, 859880, 71 [C7x_1 ] 68721.911030 s: 0.078, 859880, 72 [C7x_1 ] 68721.911057 s: 0.097, 859880, 73 [C7x_1 ] 68721.911085 s: 0.104, 859880, 74 [C7x_1 ] 68721.911113 s: 0.261, 960360, 75 [C7x_1 ] 68721.911141 s: 0.029, 730728, 76 [C7x_1 ] 68721.911167 s: 0.065, 831208, 77 [C7x_1 ] 68721.911195 s: 0.036, 831208, 78 [C7x_1 ] 68721.911222 s: 0.268, 831208, 79 [C7x_1 ] 68721.911249 s: 0.036, 831208, 80 [C7x_1 ] 68721.911276 s: 0.268, 831208, 81 [C7x_1 ] 68721.911303 s: 0.065, 931688, 82 [C7x_1 ] 68721.911330 s: 0.029, 730728, 83 [C7x_1 ] 68721.911358 s: 0.124, 931560, 84 [C7x_1 ] 68721.911385 s: 0.073, 845544, 85 [C7x_1 ] 68721.911412 s: 0.348, 960360, 86 [C7x_1 ] 68721.911439 s: 0.349, 845544, 87 [C7x_1 ] 68721.911467 s: 0.044, 960360, 88 [C7x_1 ] 68721.911494 s: 0.014, 845544, 89 [C7x_1 ] 68721.911522 s: 0.000, 845544, 90 [C7x_1 ] 68721.911551 s: 0.348, 960360, 91 [C7x_1 ] 68721.911580 s: 0.014, 845544, 92 [C7x_1 ] 68721.911608 s: 0.000, 845544, 93 [C7x_1 ] 68721.911636 s: 0.348, 960360, 94 [C7x_1 ] 68721.911665 s: 0.022, 845544, 95 [C7x_1 ] 68721.911694 s: 0.000, 845544, 96 [C7x_1 ] 68721.911723 s: 0.348, 845544, 97 [C7x_1 ] 68721.911751 s: 0.022, 730728, 98 [C7x_1 ] 68721.911779 s: 0.000, 730728, 99 [C7x_1 ] 68721.911808 s: 0.061, 935656, 100 [C7x_1 ] 68721.911837 s: 0.282, 935656, 101 [C7x_1 ] 68721.911865 s: 0.035, 935656, 102 [C7x_1 ] 68721.911892 s: 0.000, 935656, 103 [C7x_1 ] 68721.911921 s: 0.281, 935656, 104 [C7x_1 ] 68721.911957 s: 0.021, 935656, 105 [C7x_1 ] 68721.911987 s: 0.000, 935656, 106 [C7x_1 ] 68721.912016 s: 0.021, 730728, 107 [C7x_1 ] 68721.912044 s: 0.000, 730728, 108 [C7x_1 ] 68721.912072 s: 0.037, 730728, 109 [C7x_1 ] 68721.912101 s: 0.000, 730728, 110 [C7x_1 ] 68721.912129 s: 0.061, 935656, 111 [C7x_1 ] 68721.912158 s: 0.282, 935656, 112 [C7x_1 ] 68721.912185 s: 0.282, 935656, 113 [C7x_1 ] 68721.912212 s: 0.060, 935656, 114 [C7x_1 ] 68721.912240 s: 0.037, 935656, 115 [C7x_1 ] 68721.912268 s: 0.000, 935656, 116 [C7x_1 ] 68721.912297 s: 0.282, 935656, 117 [C7x_1 ] 68721.912325 s: 0.037, 935656, 118 [C7x_1 ] 68721.912353 s: 0.000, 935656, 119 [C7x_1 ] 68721.912382 s: 0.282, 935656, 120 [C7x_1 ] 68721.912410 s: 0.044, 935656, 121 [C7x_1 ] 68721.912438 s: 0.000, 935656, 122 [C7x_1 ] 68721.912467 s: 0.281, 935656, 123 [C7x_1 ] 68721.912495 s: 0.036, 730728, 124 [C7x_1 ] 68721.912523 s: 0.000, 730728, 125 [C7x_1 ] 68721.912552 s: 0.065, 420456, 126 [C7x_1 ] 68721.912581 s: 0.268, 834280, 127 [C7x_1 ] 68721.912609 s: 0.268, 420456, 128 [C7x_1 ] 68721.912636 s: 0.059, 834280, 129 [C7x_1 ] 68721.912663 s: 0.036, 420456, 130 [C7x_1 ] 68721.912691 s: 0.000, 420456, 131 [C7x_1 ] 68721.912719 s: 0.268, 834280, 132 [C7x_1 ] 68721.912748 s: 0.036, 420456, 133 [C7x_1 ] 68721.912776 s: 0.000, 420456, 134 [C7x_1 ] 68721.912805 s: 0.268, 834280, 135 [C7x_1 ] 68721.912834 s: 0.064, 420456, 136 [C7x_1 ] 68721.912862 s: 0.000, 420456, 137 [C7x_1 ] 68721.912890 s: 0.268, 420456, 138 [C7x_1 ] 68721.912917 s: 0.064, 6632, 139 [C7x_1 ] 68721.912952 s: 0.000, 0, 140 [C7x_1 ] 68721.913097 s: TIDL_initializeHandleForPreemption is completed [C7x_1 ] 68721.920105 s: ============================= [C7x_1 ] 68721.920128 s: pConfig->inPadL:0 [C7x_1 ] 68721.920146 s: pConfig->inPadR:0 [C7x_1 ] 68721.920162 s: pConfig->inPadT:0 [C7x_1 ] 68721.920177 s: pConfig->inPadB:0 [C7x_1 ] 68721.920194 s: pConfig->inWidth:800 [C7x_1 ] 68721.920211 s: pConfig->inHeight:512 [C7x_1 ] 68721.920229 s: ============================= [C7x_1 ] 68722.085419 s: L:0:0 [C7x_1 ] 68722.085440 s: L:20:0 [C7x_1 ] 68722.085457 s: L:40:0 [C7x_1 ] 68722.085473 s: L:60:0 [C7x_1 ] 68722.085489 s: L:80:0 [C7x_1 ] 68722.085505 s: L:100:0 [C7x_1 ] 68722.085521 s: L:120:0 [C7x_1 ] 68722.085536 s: L:140:0 [C7x_1 ] 68722.085552 s: L:160:0 [C7x_1 ] 68722.085567 s: L:180:0 [C7x_1 ] 68722.085583 s: L:200:0 [C7x_1 ] 68722.085599 s: L:220:0 [C7x_1 ] 68722.085614 s: L:240:0 [C7x_1 ] 68722.085630 s: L:260:0 [C7x_1 ] 68722.085645 s: L:280:0 [C7x_1 ] 68722.085661 s: L:300:0 [C7x_1 ] 68722.085677 s: L:320:0 [C7x_1 ] 68722.085692 s: L:340:0 [C7x_1 ] 68722.085708 s: L:360:0 [C7x_1 ] 68722.085724 s: L:380:0 [C7x_1 ] 68722.085739 s: L:400:0 [C7x_1 ] 68722.085755 s: L:420:0 [C7x_1 ] 68722.085770 s: L:440:0 [C7x_1 ] 68722.085786 s: L:460:0 [C7x_1 ] 68722.085802 s: L:480:0 [C7x_1 ] 68722.085817 s: L:500:0 [C7x_1 ] 68722.085833 s: L:520:0 [C7x_1 ] 68722.085848 s: L:540:0 [C7x_1 ] 68722.085864 s: L:560:0 [C7x_1 ] 68722.085880 s: L:580:0 [C7x_1 ] 68722.085895 s: L:600:0 [C7x_1 ] 68722.085911 s: L:620:0 [C7x_1 ] 68722.085926 s: L:640:0 [C7x_1 ] 68722.085942 s: L:660:0 [C7x_1 ] 68722.085967 s: L:680:0 [C7x_1 ] 68722.085984 s: L:700:0 [C7x_1 ] 68722.086000 s: L:720:0 [C7x_1 ] 68722.086015 s: L:740:0 [C7x_1 ] 68722.086031 s: L:760:0 [C7x_1 ] 68722.086047 s: L:780:0 [C7x_1 ] 68722.086063 s: L:800:0 [C7x_1 ] 68722.086078 s: L:820:0 [C7x_1 ] 68722.086094 s: L:840:0 [C7x_1 ] 68722.086110 s: L:860:0 [C7x_1 ] 68722.086125 s: L:880:0 [C7x_1 ] 68722.086141 s: L:900:0 [C7x_1 ] 68722.086156 s: L:920:0 [C7x_1 ] 68722.086172 s: L:940:0 [C7x_1 ] 68722.086187 s: L:960:0 [C7x_1 ] 68722.086203 s: L:980:0 [C7x_1 ] 68722.086219 s: L:1000:0 [C7x_1 ] 68722.086235 s: L:1020:0 [C7x_1 ] 68722.086275 s: A0 =0x0000000000000000 A1 =0x0000000000000000 [C7x_1 ] 68722.086310 s: A2 =0x0000000000000000 A3 =0x0000000000000000 [C7x_1 ] 68722.086344 s: A4 =0x0000000000000000 A5 =0x0000000000000000 [C7x_1 ] 68722.086376 s: A6 =0x0000000000000000 A7 =0x0000000000000000 [C7x_1 ] 68722.086408 s: A8 =0x0000000000000000 A9 =0x0000000000000000 [C7x_1 ] 68722.086439 s: A10=0x0000000000000000 A11=0x0000000000000000 [C7x_1 ] 68722.086470 s: A12=0x0000000000000000 A13=0x0000000000000000 [C7x_1 ] 68722.086501 s: A14=0x0000000000000000 A15=0x0000000000000000 [C7x_1 ] 68722.086533 s: D0 =0x0000000000000000 D1 =0x0000000000000000 [C7x_1 ] 68722.086565 s: D2 =0x0000000000000000 D3 =0x0000000000000000 [C7x_1 ] 68722.086595 s: D4 =0x0000000000000000 D5 =0x0000000000000000 [C7x_1 ] 68722.086628 s: D6 =0x0000000000000000 D7 =0x0000000000000000 [C7x_1 ] 68722.086660 s: D8 =0x0000000000000000 D9 =0x0000000000000000 [C7x_1 ] 68722.086692 s: D10=0x0000000000000000 D11=0x0000000000000000 [C7x_1 ] 68722.086723 s: D12=0x0000000000000000 D13=0x0000000000000000 [C7x_1 ] 68722.086754 s: D14=0x0000000000000000 D15=0x0000000000000000 [C7x_1 ] 68722.086785 s: AM0=0x0000000000000000 AM1=0x0000000000000000 [C7x_1 ] 68722.086816 s: AM2=0x0000000000000000 AM3=0x0000000000000000 [C7x_1 ] 68722.086848 s: AM4=0x0000000000000000 AM5=0x0000000000000000 [C7x_1 ] 68722.086878 s: AM6=0x0000000000000000 AM7=0x0000000000000000 [C7x_1 ] 68722.086910 s: AL0=0x0000000000000000 AL1=0x0000000000000000 [C7x_1 ] 68722.086942 s: AL2=0x0000000000000000 AL3=0x0000000000000000 [C7x_1 ] 68722.086974 s: AL4=0x0000000000000000 AL5=0x0000000000000000 [C7x_1 ] 68722.087005 s: AL6=0x0000000000000000 AL7=0x0000000000000000 [C7x_1 ] 68722.087037 s: P0=0x000000000000003f P1=0x00000000000afb7a [C7x_1 ] 68722.087074 s: P2=0x00000000046842f8 P3=0x00000000cc8377ff [C7x_1 ] 68722.087109 s: P4=0x00000000001014b5 P5=0x000000000840b5ba [C7x_1 ] 68722.087145 s: P6=0x000000004875caf3 P7=0x000000000358c802 [C7x_1 ] 68722.087178 s: FPCR=0x0000000000000010 FSR=0x0000000000000000 [C7x_1 ] 68722.087213 s: GFPGFR=0x000000000700001d GPLY=0x0000000000000000 [C7x_1 ] 68722.087234 s: [C7x_1 ] 68722.087262 s: VBM0=0x0000000000000000 [0] VBM1=0x0000000000000000 [0] [C7x_1 ] 68722.087301 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.087338 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.087374 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.087410 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.087446 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.087482 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.087518 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.087540 s: [C7x_1 ] 68722.087566 s: VBM2=0x0000000000000000 [0] VBM3=0x0000000000000000 [0] [C7x_1 ] 68722.087602 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.087638 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.087675 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.087712 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.087748 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.087783 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.087818 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.087839 s: [C7x_1 ] 68722.087866 s: VBM4=0x0000000000000000 [0] VBM5=0x0000000000000000 [0] [C7x_1 ] 68722.087903 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.087939 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.087974 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.088010 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.088046 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.088082 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.088117 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.088138 s: [C7x_1 ] 68722.088165 s: VBM6=0x0000000000000000 [0] VBM7=0x0000000000000000 [0] [C7x_1 ] 68722.088209 s: 0x0000000000000000 [1] 0x091000010100ff03 [1] [C7x_1 ] 68722.088245 s: 0x0000000000000000 [2] 0x0000000000000009 [2] [C7x_1 ] 68722.088284 s: 0x0000000000000000 [3] 0x00000000a1008020 [3] [C7x_1 ] 68722.088320 s: 0x0000000000000000 [4] 0x0000000000003fe0 [4] [C7x_1 ] 68722.088356 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.088391 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.088427 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.088447 s: [C7x_1 ] 68722.088477 s: VBL0=0x0000000000000000 [0] VBL1=0x0000000099d0d8a8 [0] [C7x_1 ] 68722.088517 s: 0x0000000000011002 [1] 0x0000000099d0da30 [1] [C7x_1 ] 68722.088555 s: 0x0000000000000007 [2] 0x0000000099ddcc78 [2] [C7x_1 ] 68722.088593 s: 0x000000000000e001 [3] 0x0000000000001802 [3] [C7x_1 ] 68722.088634 s: 0x0000000099c1bb90 [4] 0x0000000099de5af0 [4] [C7x_1 ] 68722.088675 s: 0x00000000a1042400 [5] 0x0000000099ddd038 [5] [C7x_1 ] 68722.088717 s: 0x00000000b2000040 [6] 0x000000009a411d08 [6] [C7x_1 ] 68722.088754 s: 0x0000000000000210 [7] 0x0000000000000410 [7] [C7x_1 ] 68722.088774 s: [C7x_1 ] 68722.088810 s: VBL2=0x0000000000000030 [0] VBL3=0xc09302812c804161 [0] [C7x_1 ] 68722.088857 s: 0x0000000000000601 [1] 0x8800202012110f00 [1] [C7x_1 ] 68722.088911 s: 0xc1003d0145004710 [2] 0x9201440000600063 [2] [C7x_1 ] 68722.088957 s: 0x61080c108f14036a [3] 0x0000000000000fd8 [3] [C7x_1 ] 68722.089004 s: 0x20000280e9081080 [4] 0x0000000099d0da70 [4] [C7x_1 ] 68722.089048 s: 0x08241452cc141000 [5] 0x0000000000000014 [5] [C7x_1 ] 68722.089087 s: 0x0000000099d0d8a8 [6] 0x0000000000000034 [6] [C7x_1 ] 68722.089129 s: 0x0000000099d0d8a8 [7] 0x0000000099c1b808 [7] [C7x_1 ] 68722.089149 s: [C7x_1 ] 68722.089186 s: VBL4=0x0000000000000003 [0] VBL5=0x2020202020202020 [0] [C7x_1 ] 68722.089232 s: 0x0000000000000fa8 [1] 0x2020202020202020 [1] [C7x_1 ] 68722.089278 s: 0x0000000000000fb0 [2] 0x2020202020202020 [2] [C7x_1 ] 68722.089323 s: 0x0000000000000000 [3] 0x170b780258613209 [3] [C7x_1 ] 68722.089362 s: 0x0000000000003fe0 [4] 0x0000000099de40f8 [4] [C7x_1 ] 68722.089407 s: 0x0000000000000000 [5] 0x1491ac0290002004 [5] [C7x_1 ] 68722.089452 s: 0x0000000000000410 [6] 0x7054c04862120a48 [6] [C7x_1 ] 68722.089497 s: 0xcc2a005112928221 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.089517 s: [C7x_1 ] 68722.089545 s: VBL6=0x0000000000000000 [0] VBL7=0x0000000000000000 [0] [C7x_1 ] 68722.089581 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.089617 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.089663 s: 0x0000000000003fe0 [3] 0xffffffffffffffd0 [3] [C7x_1 ] 68722.089699 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.089735 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.089770 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.089806 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.089826 s: [C7x_1 ] 68722.089853 s: VB0=0x0000000000000000 [0] VB1=0x0000000000000000 [0] [C7x_1 ] 68722.089889 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.089925 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.089961 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.089997 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.090033 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.090069 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.090104 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.090125 s: [C7x_1 ] 68722.090152 s: VB2=0x0000000000000000 [0] VB3=0x0000000000000000 [0] [C7x_1 ] 68722.090188 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.090225 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.090262 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.090298 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.090334 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.090370 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.090407 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.090428 s: [C7x_1 ] 68722.090454 s: VB4=0x0000000000000000 [0] VB5=0x0000000000000000 [0] [C7x_1 ] 68722.090490 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.090526 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.090563 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.090599 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.090635 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.090670 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.090707 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.090727 s: [C7x_1 ] 68722.090753 s: VB6=0x0000000000000000 [0] VB7=0x0000000000000000 [0] [C7x_1 ] 68722.090789 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.090826 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.090863 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.090898 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.090934 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.090970 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.091006 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.091026 s: [C7x_1 ] 68722.091053 s: VB8=0x0000000000000000 [0] VB9=0x0000000000000000 [0] [C7x_1 ] 68722.091089 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.091125 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.091161 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.091197 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.091232 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.091269 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.091304 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.091325 s: [C7x_1 ] 68722.091352 s: VB10=0x0000000000000000 [0] VB11=0x0000000000000000 [0] [C7x_1 ] 68722.091389 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.091425 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.091461 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.091498 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.091534 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.091569 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.091605 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.091626 s: [C7x_1 ] 68722.091653 s: VB12=0x0000000000000000 [0] VB13=0x0000000000000000 [0] [C7x_1 ] 68722.091690 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.091726 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.091762 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.091798 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.091834 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.091870 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.091905 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.091926 s: [C7x_1 ] 68722.091953 s: VB14=0x0000000000000000 [0] VB15=0x0000000000000000 [0] [C7x_1 ] 68722.091989 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.092026 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.092061 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.092098 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.092134 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.092169 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.092205 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.092226 s: [C7x_1 ] 68722.092271 s: CUCR0=0x288ab346ca00b86b [0] CUCR1=0x88b03a722914994d [0] [C7x_1 ] 68722.092324 s: 0x004d05df00e22420 [1] 0x7922822e1a008018 [1] [C7x_1 ] 68722.092379 s: 0xd5882a1680164810 [2] 0xa07e848350389040 [2] [C7x_1 ] 68722.092420 s: 0x000000000840b5ba [3] 0x000000000358c802 [3] [C7x_1 ] 68722.092474 s: 0xa5a000008a910190 [4] 0x190ea8249da80d10 [4] [C7x_1 ] 68722.092528 s: 0x0420891050840605 [5] 0xd8b53d6344b32007 [5] [C7x_1 ] 68722.092583 s: 0xc9201c714d6a0b8f [6] 0xa2c1c108331b01e0 [6] [C7x_1 ] 68722.092624 s: 0x00000000001014b5 [7] 0x000000004875caf3 [7] [C7x_1 ] 68722.092644 s: [C7x_1 ] 68722.092689 s: CUCR2=0x20c0a80a1ea20242 [0] CUCR3=0xc908140875009220 [0] [C7x_1 ] 68722.092744 s: 0x1818865464420485 [1] 0xe042028896210724 [1] [C7x_1 ] 68722.092799 s: 0x560098259cc22170 [2] 0x219b0c15000e0801 [2] [C7x_1 ] 68722.092836 s: 0x000000000000081c [3] 0x0000000000000009 [3] [C7x_1 ] 68722.092890 s: 0x1c05119c408608e8 [4] 0x252208a84d01d1c0 [4] [C7x_1 ] 68722.092945 s: 0xb840441290081813 [5] 0xb277422920080070 [5] [C7x_1 ] 68722.092999 s: 0x9890018a20165080 [6] 0xb4a3010a02105850 [6] [C7x_1 ] 68722.093036 s: 0x0000000000000824 [7] 0x0000000000000804 [7] [C7x_1 ] 68722.093057 s: [C7x_1 ] 68722.093087 s: SE0_0=0x0000000000000000 [0] SE0_1=0x00000000a3d24000 [0] [C7x_1 ] 68722.093127 s: 0x0000000000000000 [1] 0x00000000a3d24000 [1] [C7x_1 ] 68722.093163 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.093202 s: 0x00000000a3d24000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.093240 s: 0x00000000a3d24000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.093279 s: 0x00000000a3d24000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.093325 s: 0x00000000a3d24000 [6] 0x0012c0000012c000 [6] [C7x_1 ] 68722.093371 s: 0x00000000a3d24000 [7] 0x0012c0000012c000 [7] [C7x_1 ] 68722.093392 s: [C7x_1 ] 68722.093419 s: SE0_2=0x0000000000000000 [0] SE0_3=0x0000000000000000 [0] [C7x_1 ] 68722.093455 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.093491 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.093529 s: 0x000000000012c000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.093565 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.093601 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.093637 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.093672 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.093693 s: [C7x_1 ] 68722.093721 s: SE1_0=0x0000000000000000 [0] SE1_1=0x0000000000000000 [0] [C7x_1 ] 68722.093758 s: 0x0000000000000000 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.093794 s: 0x0000000000000000 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.093830 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.093866 s: 0x0000000000000000 [4] 0x0000000000000000 [4] [C7x_1 ] 68722.093902 s: 0x0000000000000000 [5] 0x0000000000000000 [5] [C7x_1 ] 68722.093937 s: 0x0000000000000000 [6] 0x0000000000000000 [6] [C7x_1 ] 68722.093973 s: 0x0000000000000000 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.093994 s: [C7x_1 ] 68722.094031 s: SE1_2=0x0000000000000000 [0] SE1_3=0x81577583a1ad2427 [0] [C7x_1 ] 68722.094077 s: 0x0000000000000000 [1] 0xaef6d5eba3d60412 [1] [C7x_1 ] 68722.094122 s: 0x0000000000000000 [2] 0x26204708d0250018 [2] [C7x_1 ] 68722.094159 s: 0x0000000000000000 [3] 0x0000000000000808 [3] [C7x_1 ] 68722.094213 s: 0xd3cdcc952238aeaa [4] 0x9fa1e310f1e83d86 [4] [C7x_1 ] 68722.094266 s: 0x1ba9d94e93dd080a [5] 0x115e9cfb7f3ce77d [5] [C7x_1 ] 68722.094320 s: 0x9e2b948e4cc0d000 [6] 0xed4014481a090301 [6] [C7x_1 ] 68722.094358 s: 0x0000000000000800 [7] 0x0000000000000000 [7] [C7x_1 ] 68722.094378 s: [C7x_1 ] 68722.094415 s: SA0CR=0xe14378a04a004102 [0] SA1CR=0x0000000000000000 [0] [C7x_1 ] 68722.094460 s: 0xc8044200225121b0 [1] 0x0000000000000000 [1] [C7x_1 ] 68722.094506 s: 0x4880000241c82080 [2] 0x0000000000000000 [2] [C7x_1 ] 68722.094551 s: 0xec23bb6653795bc8 [3] 0x0000000000000007 [3] [C7x_1 ] 68722.094604 s: 0x0401000231400048 [4] 0x0b3011111500023d [4] [C7x_1 ] 68722.094659 s: 0xa8097520904829a0 [5] 0xa929422000590179 [5] [C7x_1 ] 68722.094713 s: 0x3a898414d0030000 [6] 0x6145001149284803 [6] [C7x_1 ] 68722.094767 s: 0x19ac17f6a02d2a6c [7] 0xd432ec7e3dbf0474 [7] [C7x_1 ] 68722.094788 s: [C7x_1 ] 68722.094826 s: SA2CR=0x0000000000000000 [0] SA3CR=0x235fee4e488c8710 [0] [C7x_1 ] 68722.094872 s: 0x0000000000000000 [1] 0xf3053c50844851f5 [1] [C7x_1 ] 68722.094918 s: 0x0000000000000000 [2] 0x6471dbe227290190 [2] [C7x_1 ] 68722.094955 s: 0x00000000000012c0 [3] 0x000000000000003c [3] [C7x_1 ] 68722.095001 s: 0x0000000000000040 [4] 0x75134d898210c3ae [4] [C7x_1 ] 68722.095047 s: 0x0000000000000040 [5] 0xffc50104c1c98ab2 [5] [C7x_1 ] 68722.095093 s: 0x0000000000000040 [6] 0x1108d9b88080c105 [6] [C7x_1 ] 68722.095132 s: 0x00000000cccccccd [7] 0x0000000000000006 [7] [C7x_1 ] 68722.095152 s: [C7x_1 ] 68722.095199 s: SA0CNTR0=0x9a21112c03110811 [0] SA1CNTR0=0xffbffd7fdfd77ffb [0] [C7x_1 ] 68722.095255 s: 0x6209b0204212102c [1] 0xfdda7c7ff7fb7feb [1] [C7x_1 ] 68722.095309 s: 0x170b780258613209 [2] 0xddfefffbbf97bdef [2] [C7x_1 ] 68722.095346 s: 0x0000000000000000 [3] 0x0000000000000000 [3] [C7x_1 ] 68722.095399 s: 0x026fa81701210be2 [4] 0x1491ac0290002004 [4] [C7x_1 ] 68722.095454 s: 0xb814514400994004 [5] 0x7054c04862120a48 [5] [C7x_1 ] 68722.095508 s: 0x62008c6000a95454 [6] 0x242605714099102a [6] [C7x_1 ] 68722.095549 s: 0x0000000000000001 [7] 0x00000340000000d0 [7] [C7x_1 ] 68722.095570 s: [C7x_1 ] 68722.095615 s: SA2CNTR0=0xc480e10508000258 [0] SA3CNTR0=0x020600122d202600 [0] [C7x_1 ] 68722.095671 s: 0x96857190800440a7 [1] 0xc442411600860110 [1] [C7x_1 ] 68722.095722 s: 0xc151700204001400 [2] 0x00001824270ed28a [2] [C7x_1 ] 68722.095769 s: 0x0000000000000028 [3] 0x3401eeeb29b37fa6 [3] [C7x_1 ] 68722.095823 s: 0x1012908082401904 [4] 0x58081188020c0008 [4] [C7x_1 ] 68722.095878 s: 0x62a160210d501305 [5] 0xf90481080844e5d0 [5] [C7x_1 ] 68722.095931 s: 0x0201e7000007c000 [6] 0x1340ca70d0a00000 [6] [C7x_1 ] 68722.095967 s: 0x000000000000000a [7] 0x0000000000000000 [7] [C7x_1 ] 68722.095988 s: [C7x_1 ] 68722.096012 s: Exception at 0x000000009a0707f8 [C7x_1 ] 68722.096043 s: TSR at time of exception: 0x000000000300ff03 [C7x_1 ] 68722.096066 s: Internal exception: [C7x_1 ] 68722.096089 s: IERR=0x0000000000000400 [C7x_1 ] 68722.096112 s: IEAR=0x000000009a0707f8 [C7x_1 ] 68722.096134 s: IESR=0x0000000000000801 [C7x_1 ] 68722.096154 s: Data fetch exception [C7x_1 ] 68722.096179 s: cpu_dmc_X_rstatus[2:0]=0x1
this is A53 print log:
may you see the problem. thank you
Hello Yang Yong,
Your goal here is to print the input tensor, correct?
From what I'm seeing, it looks like there is effectively a seg-fault happening here. The code looks like it is not referencing the correct memory within the function you have outlined. I also don't see anything in the log printing the inTensor->mem_size, whereas there should be a printf doing this.
I am concerned that the pointer to the tensor_uint8_buffer is not correct, so it's hitting an error when you go beyond 1024 bytes.
This portion of the code base is not generally supported by our team so I can only provide limited input here.
BR,
Reese