This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816x Benchmarks?



Hello,

 

I'm looking for DM816x benchmarks, I have 2 pipelines(at the end) to implement with DM816x. I wonder:

 

1) are they possible with DM816x?

2) if they are, do you have any CPU/DSP usage estimation for these pipelines?

3) Can I add any HDMI output capabilities in these pipelines without affecting performance?

 

Thanks in advance,

Caglar

 

=== Pipeline 1 ===

                                                                                       -----------> save to HDD using SATA

                                                   -----------> Encode 

                                                                                      -----------> transfer over Gigabit EMAC

16-bit 30 fps 720p capture  

                                                  -----------> transfer over Gigabit EMAC(~450Mbps)

 

=== Pipeline 2 ===

 

-----------> save to HDD using SATA

~900 Mbps transfer over Gigabit Emac -----------> Encode 

                    -----------> Transfer over EMAC