Other Parts Discussed in Thread: FLASHTOOL, AM3505
I'm trying to use UART3 with FlashTool V1.6 on my custom AM35XX hardware. Since I am using Micron NAND Flash and DDR2 SDRAM I am using the default config file.
When I turn on my custom hardware FlashTool gets to :
Please turn off device, then turn it on again ¯ Awaiting ASIC id After re-cycling power or pressing reset the session times out. When I however use to OTG device port with the USB FlashTool setting I get the ASIC ID and other information and the *.bin file is downloaded. It would appear that I am having issues with UART3 and the 232 transceiver but after reviewing the schematic everything looks OK. Are there any suggestions as to what I can check to get UART3 working? Also, I cannot boot from an SD Card using MMC2 I am using the SNAVCA406E Transceiver. I am setting the Boot Parms. for MMC2. Do the direction control signals for the transceiver require pull-ups or does the processor takes care of direction control on power up so it can read the SD Card?