Other Parts Discussed in Thread: TMS320C6678
Hi,
I cannot use the C6678 IBIS file (tms320C6678_4_2_1_r1p5b.ibs) with HyperLynx 8.1.1.
When I try to select the model I get the following error message:
"Differential pin N1 is paired with a NC pin in component tms320c6678_4_2_1 of file tms320C6678_4_2_1_r1p5b.ibs"
It then says the "selected device is unusable".
Looking at the IBIS file, all serdes pins are set to NC including the MCM one on pin N1. I assume this is because the IBIS file doesn't model these high-speed pins. Yet I notice that pin N1 is also referenced lower down in the file saying it is a differential pin that is paired with M1, another NC. Should this differential pairing be here. If they're NC then they should be NC shouldn't they?
I don't actually want to model the serdes pins, but this error stops me from accessing any pins. Anyone else got this to work with HyperLynx?
Richard