Part Number: TDA4AH-Q1
Hi TI Experts,
Can you tell me what needs to be set or configured additionally for the USB gadget driver to be recognized by windows for the u-boot booting from eg SD card or qspi Nor Flash on j784S4 EVM?
I want to note that booting via USB0 works descripted here:
3.1.1.2. USB Device Firmware Upgrade (DFU) — Processor SDK Linux for J784s4 Documentation
And when u-boot is finally running in this usb boot mode then usb gadget driver is recognized by windows and dfu-utlis works (eg for dfu and qspi or emmc)
But when the same SPL-Uboot is booted from SD card or QSPI Nor flash the usb gadget driver is not recognized and that dfu-utils not works as descripted in:
3.1.1.7. OSPI/QSPI — Processor SDK Linux for J784s4 Documentation
There is no errors in U-boot - looks like usb works but windows not recognize it.
SW2 switch 3 and 4 are set eg to ON ON. But looks like RBL USB boot mode also works for SW2 3-OFF and 4-OFF. Maybe here is something to be set correctly...But looks like in case of RBL USB mode usb0 path is set correctly.
I also try to set CONFIG_DFU_OVER_USB=y in A72 and R5 defconfigs - and not help .
Lates SPL/uboot version is used from ti-processor-sdk-linux-adas-j784s4-evm-09_01_00_06.
Regards
Dariusz Gasiorowski