I just plug in a marvell SD card, it detects it, but in which directory I should put the sd8686.bin, sd8686_helper.bin
right now is in the /lib/modules/2.6.32.17-davinci1/source/firmware but cant detected there, how can I find out the path that is set for the drivers?
mmc0: new SDIO card at address 0001
libertas_sdio mmc0:0001:1: firmware: requesting sd8686_helper.bin
libertas: can't load helper firmware
libertas: failed to load helper firmware
libertas_sdio: probe of mmc0:0001:1 failed with error -2