Part Number: PROCESSOR-SDK-J721S2
Board: Customer equips J721s2
BSP: 8.6
Refer to the URL: e2e.ti.com/.../4668565
"... Before calling GPIO Init, define gpioPinConfigs[] with PIN | DIR.
"Where PIN should be a hexadecimal value 0xABCD
Where AB represents Port number and CD represents the Pin number. For example, for configuring WKUP_GPIO0_16: PIN = 0x0010"
Question: once we declare 0x0010 through GPIO_DEVICE_CONFIG() function, how system can tell whether the gpio pin is WKUP_GPIO0_16, not GPIO0_16?
- Wilson