Setup :
Board : J784s4_evm
Test on processors R5F : mcu2_0 and mcu2_1 and mpu : A72
SDK version : 9.01
OS I use : Ubuntu 22.04.4
Test : with SD card boot
Context :
Hello,
I'm currently searching to activate and try all 8 externals ports of the CPSW_9g switch.
For that purpose I use two externals QPEnet extension boards, connected to the card.
I tried in first place the default Ethfw application with only one QPEnet on the first emplacement, which work well. But when I tried to extend my experiment to the seconde Eth. expan. connector, by modifying the firmware the QPEnet doesn't respond at all.
This lead me to wonder :Is it possible to connect two QPEnet simultaniously ?
Ether way is there a procedure to follow to activate the Eth. expan. connector 2 other than including the port in the mcu application ?
In addition I wish to add the other R5F mcu to the network (and C7x if possible), connected at the same time; is it possible ? and if yes, is there a documentation to follow ?
Thank you in advance and if you have any question, please ask.
Regards,
Matthias