Part Number: SK-AM62P-LP
Other Parts Discussed in Thread: AM62P
Hi,
We are currently conducting performance tests on the board running AOSP 14. (https://software-dl.ti.com/processor-sdk-android/esd/AM62PX/09_01_00/docs/devices/AM62PX/android/index.html#) We are using the TouchLatency app from AOSP at /framework/base/tests/TouchLatency. When monitoring the CPU usage with top, we observe that the app itself consumes about 30~40% of a CPU at all times. We performed the same test on a previous platform with jacinto6 and noticed a consumption of about 8%.

We also conducted another test using a map application, where the idle consumption was around 1%, and the performance was poor.
Q1. Are we missing something when it comes to handling applications on Android? Is there any configuration we should be aware of?
Thank you.
Ivan Simonavicius