Other Parts Discussed in Thread: OMAP-L137
On boot, I get this message:
EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended
During power cycle tests, the SD card gets corrupted, corrupted nodes are noted on bootup. I would like to run e2fsck on every bootup but I can't find the where to enable that. I've checked the usual suspects:
/etc/fstab
rootfs / auto defaults 1 1
/etc/default/rcS
ENABLE_ROOTFS_FSCK=yes
Environment:
OMAP-L137 EVM from Spectrum Digital
DVSDK 03.21.00.04 aka linux2.6.37
Arago FS 2009-11 on SD Card.