This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: OTP Keys Certificate

Part Number: PROCESSOR-SDK-AM64X


Hello,

I have two questions :

1. SWREV fields : COARDCONFIG, SBL and SYSFW are these for the TI usage and not related to customer's application software revision ?

    Is there any field in the Customer's OTP that can be used for application SW revision ? Or is it already part of magic number in the Application Certificate ?

    In that case the new update of application software has nothing to do with the OTP and do not worry about writing any application revision to this OTP area ?

2. OTP Keys Certificate : is this one -to- one to CPU when the certificate is generated and cannot be used to other CPU (KEK is RGN for each CPU)?

So customer's keys should be programmed using the KW when the certificate is generated together ?

3. Can the keys be programmed later using the pre-generated OTP Keys Certificate (it's certificate) ? 

4. For the best practical production should the blank CPU (HS-FS) to be programmed with the keys (HS-SE) before sending to the assembly house ?

    This question is for the reason of keys protection which CPU cannot be programmed at the outside assembly house.

    Any recommendation fixture with special socket for this purpose to pre=program the keys before assembly ?

Regards;

Huynh