Part Number: AM625
Command: aplay jiewo.wav
Platform: AM625 SDK 9.0 SDK8.3
Issue:In SDK9.0,when TF card and U disk are plugged into the development board at the same time, audio playback will have a probability of failure.The probability of failure is about 50%.The errors are as follows:
root@OK62xx:/# aplay jiewo.wav
aplay: main:831: audio open error: Invalid argument
On the same embedded card, SDK8.3 does not have this problem.Therefore, hardware problems can be ruled out.
Please help me to complete the task.
Thanks,
Xiong wei