This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: [Q] How do I set up video1, video2....video8 for DS90UB960

Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM

Dear,

It's our block diagram.

As you see, we use the 8 camera, and It's connected to TDA4VM CSI port through DS90UB960.

                            ( camera1, camera2, camera3, .....,  camera 8 )

Also, we use the processor SDK linux for J721e 09.01.00 version.

Then, I use the DS90UB960 linux driver and device tree (dts ) in this SDK.

But, I don't know " How do I set up video1, video2, video3,..... video 8 for DS90UB960 "

I want the video1 to connect to the camera1, also the video2 to connect to the camera2,  etc.... 

Also, the video1 is linux device like " /dev/video1" 

Please, let me know that.

best regards,

hosung shin.