Part Number: TDA4VM
Hi,
I'm trying to compile a custom model on PC(x86) - Ubuntu 22.04 using edgeai_tidl_tools(latest - 26/03/24).
I'm facing an issue on this, the inference doesn't halt. It is frozen after ******* In TIDL_subgraphRtInvoke ******** .
In TIDL_runtimesPostProcessNet 4 ************ in TIDL_subgraphRtCreate ************ The soft limit is 2048 The hard limit is 2048 MEM: Init ... !!! MEM: Init ... Done !!! 0.0s: VX_ZONE_INIT:Enabled 0.1s: VX_ZONE_ERROR:Enabled 0.2s: VX_ZONE_WARNING:Enabled 0.1091s: VX_ZONE_INIT:[tivxInit:185] Initialization Done !!! ************ TIDL_subgraphRtCreate done ************ ******* In TIDL_subgraphRtInvoke ******** 0 1.00000 0.00003 0.99999 6 1 1.00000 0.00003 0.99999 6 2 1.00000 0.00000 18.22760 6 3 1.00000 -22.95784 23.34633 6 4 1.00000 0.00000 18.52748 6 5 1.00000 0.00000 16.63744 6 6 1.00000 -35.66938 29.38376 6 7 1.00000 0.00000 24.47215 6 8 1.00000 0.00000 24.47215 6 9 1.00000 0.00000 24.47215 6 10 1.00000 0.00000 23.97921 6 11 1.00000 0.00000 24.47215 6 12 1.00000 0.00000 13.60912 6 13 1.00000 -21.31722 24.14623 6 14 1.00000 0.00000 13.95816 6 15 1.00000 0.00000 23.97921 6 16 1.00000 0.00000 23.97921 6 17 1.00000 0.00000 19.25303 6 18 1.00000 0.00000 23.97921 6 19 1.00000 0.00000 8.20622 6 20 1.00000 -26.19235 20.87516 6 21 1.00000 0.00000 12.56523 6 22 1.00000 0.00000 19.25303 6 23 1.00000 0.00000 19.25303 6 24 1.00000 0.00000 19.15417 6 25 1.00000 0.00000 19.25303 6 26 1.00000 0.00000 9.42462 6 27 1.00000 -15.60825 22.31817 6 28 1.00000 0.00000 12.10570 6 29 1.00000 0.00000 19.15417 6 30 1.00000 0.00000 19.15417 6 31 1.00000 -14.81230 14.13797 6 32 1.00000 0.00000 9.78303 6 33 1.00000 0.00000 13.04740 6 34 1.00000 -16.42818 13.86886 6 35 1.00000 0.00000 11.37138 6 36 1.00000 0.00000 11.37138 6 37 1.00000 0.00000 11.37138 6 38 1.00000 0.00000 10.50990 6 39 1.00000 0.00000 11.37138 6 40 1.00000 0.00000 5.87220 6 41 1.00000 -9.40662 13.79551 6 42 1.00000 0.00000 7.20522 6 43 1.00000 0.00000 10.50990 6 44 1.00000 0.00000 10.50990 6 45 1.00000 0.00000 10.50990 6 46 1.00000 0.00000 6.75473 6 47 1.00000 0.00000 5.71871 6 48 1.00000 -10.14189 16.80318 6 49 1.00000 0.00000 9.92256 6 50 1.00000 0.00000 10.50990 6 51 1.00000 0.00000 10.50990 6 52 1.00000 0.00000 10.50990 6 53 1.00000 0.00000 9.92256 6 54 1.00000 0.00000 7.31479 6 55 1.00000 -15.11326 22.41639 6 56 1.00000 0.00000 9.91941 6 57 1.00000 0.00000 10.50990 6 58 1.00000 0.00000 10.50990 6 59 1.00000 0.00000 10.50990 6 60 1.00000 0.00000 9.13293 6 61 1.00000 0.00000 6.67918 6 62 1.00000 -16.52295 16.94468 6 63 1.00000 0.00000 11.31541 6 64 1.00000 0.00000 11.31541 6 65 1.00000 0.00000 11.31541 6 66 1.00000 0.00000 10.50990 6 67 1.00000 0.00000 11.31541 6 68 1.00000 0.00000 7.29694 6 69 1.00000 -22.81109 12.59640 6 70 1.00000 0.00000 8.09317 6 71 1.00000 0.00000 10.50990 6 72 1.00000 0.00000 10.50990 6 73 1.00000 0.00000 8.01015 6 74 1.00000 0.00000 10.50990 6 75 1.00000 0.00000 5.83601 6 76 1.00000 -13.69232 13.15533 6 77 1.00000 0.00000 8.19966 6 78 1.00000 0.00000 8.19966 6 79 1.00000 0.00000 8.19966 6 80 1.00000 0.00000 7.47688 6 81 1.00000 0.00000 8.19966 6 82 1.00000 0.00000 6.35148 6 83 1.00000 -17.55709 17.04778 6 84 1.00000 0.00000 9.97488 6 85 1.00000 0.00000 9.97488 6 86 1.00000 0.00000 9.97488 6 87 1.00000 -9.28005 9.09461 6 88 1.00000 0.00000 4.69044 6 89 1.00000 0.00000 7.82371 6 90 1.00000 -13.95076 11.97064 6 91 1.00000 0.00000 9.55357 6 92 1.00000 0.00000 9.55357 6 93 1.00000 0.00000 9.55357 6 94 1.00000 0.00000 6.72975 6 95 1.00000 0.00000 9.55357 6 96 1.00000 0.00000 6.40546 6 97 1.00000 -8.62152 11.58674 6 98 1.00000 0.00000 5.68172 6 99 1.00000 0.00000 6.72975 6 100 1.00000 0.00000 6.72975 6 101 1.00000 0.00000 6.72975 6 102 1.00000 0.00000 6.19480 6 103 1.00000 0.00000 9.99279 6 104 1.00000 -10.35420 13.44050 6 105 1.00000 0.00000 10.88397 6 106 1.00000 0.00000 10.88397 6 107 1.00000 0.00000 10.88397 6 108 1.00000 0.00000 10.88397 6 109 1.00000 0.00000 7.68266 6 110 1.00000 0.00000 5.55894 6 111 1.00000 -9.88393 8.60772 6 112 1.00000 0.00000 8.46910 6 113 1.00000 0.00000 10.88397 6 114 1.00000 0.00000 10.88397 6 115 1.00000 0.00000 9.31098 6 116 1.00000 0.00000 9.31098 6 117 1.00000 -42.13771 13.04553 6 118 1.00000 -42.13771 13.04553 6 119 1.00000 -42.13771 13.04553 6 121 1.00000 -42.13771 13.04553 6 122 1.00000 -29.87323 8.82268 6 123 1.00000 -29.87323 8.82268 6
I'm attaching the onnx model, console_log file, sample onnxrt_ep.py(generated random np array for infer image) that I used, artifacts generated(incomplete) .
https://drive.google.com/drive/folders/13_nI8NE3O8tblBaT2hYWAPc-4vtmx2v_?usp=drive_link
Kindly let me know if you can help.
Note: The model runs perfectly fine in https://dev.ti.com/edgeaistudio/.
But fails in edgeai_tidl_tools setup in local PC.