Other Parts Discussed in Thread: AM62P
I'm tryng to use embeddedartist EAR00364 as my WiFi / Bluetooth module with my Board.
I've already enabled Marvell 88W8xxx PCI/PCIe Wireless support on menuconfig Device Drivers > Network device support > Wireless LAN
when i turned on the board these are the all dmesg messages with wifi.
# dmesg | grep -i wifi
[ 19.936104] init: processing action (post-fs-data) from (/system/etc/init/wifi.rc:18)
[ 19.947740] selinux: SELinux: Skipping restorecon on directory(/data/misc/apexdata/com.android.wifi)
[ 26.199610] init: starting service 'wificond'...
[ 26.218155] init: ... started service 'wificond' has pid 504
[ 38.643909] servicemanager: Could not find android.hardware.wifi.IWifi/default in the VINTF manifest.
[ 38.660641] servicemanager: Found android.hardware.wifi.supplicant.ISupplicant/default in device VINTF manifest.
[ 38.680683] servicemanager: Found android.hardware.wifi.supplicant.ISupplicant/default in device VINTF manifest.
[ 52.680884] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=0) from (/system/etc/init/wifi.rc:28)
[ 52.908720] selinux: SELinux: Could not get canonical path for /sys/kernel/debug/tracing/instances/wifi restorecon: No such file or directory.
[ 53.289815] init: Command 'mkdir /sys/kernel/tracing/instances/wifi 711' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi.rc:36) took 333ms and succeeded
[ 53.413423] init: Command 'write /sys/kernel/tracing/instances/wifi/buffer_size_kb 1' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi.rc:39) took 52ms and succeeded
[ 53.530572] init: Command 'write /sys/kernel/tracing/instances/wifi/events/net/filter name==${wifi.interface:-wlan0}' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi.rc:75) took 62ms and succeeded
[ 53.762137] init: processing action (sys.user.0.ce_available=true) from (/system/etc/init/wifi.rc:21)
[ 53.817243] selinux: SELinux: Skipping restorecon on directory(/data/misc_ce/0/apexdata/com.android.wifi)
[ 54.267080] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=1) from (/vendor/etc/init/hw/init.am62p.rc:129)
[ 54.305081] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=1 && wifi.interface=*) from (/system/etc/init/wifi.rc:98)
[ 54.498400] init: Command 'write /sys/kernel/tracing/instances/wifi/events/net/filter name==${wifi.interface}' action=sys.boot_completed=1 && sys.wifitracing.started=1 && wifi.interface=* (/system/etc/init/wifi.rc:101) took 83ms and succeeded
is there anything els that i need to do?
best regards