Part Number: TDA4AL-Q1
Hello. Ti experts.
I'm trying to libavcodec, libavutil in PSDK 9.0.0.2.
But it seems like some of the features are not supported such as AVBitStreamFilterContext type, av_register_all(), and so on.
It's supported in PSDK 8.6. So I found out if those things are in targets.
For example In PSDK8.6, AVBitStreamFilterContext is in targetfs/usr/include/libavcodec/avcode.h as below.
#if FF_API_OLD_BSF
typedef struct AVBitStreamFilterContext {
void *priv_data;
const struct AVBitStreamFilter *filter;
AVCodecParserContext *parser;
struct AVBitStreamFilterContext *next;
/**
* Internal default arguments, used if NULL is passed to av_bitstream_filter_filter().
* Not for access by library users.
*/
char *args;
} AVBitStreamFilterContext;
...
...
#endif
av_register_all() is defined in avformat.h as below.
#if FF_API_NEXT
/**
* Initialize libavformat and register all the muxers, demuxers and
* protocols. If you do not call this function, then you can select
* exactly which formats you want to support.
*
* @see av_register_input_format()
* @see av_register_output_format()
*/
attribute_deprecated
void av_register_all(void);
attribute_deprecated
void av_register_input_format(AVInputFormat *format);
attribute_deprecated
void av_register_output_format(AVOutputFormat *format);
#endif
These are in the defined option using #ifdef.
But, In targets of PSDK9.0.0.2, AVBitStreamFilterContext type, av_register_all() are not defined anywhere.
So I can't build my app which is using libavcodec.
I would like to know how to revert that libs into targetfs.
Best regards
Yongsig