This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSL library build error



hello:

      I have troubles building the csl library in ccs5.0. I installed the ccsv5.0 and the MCSDK without any error. And then follow the procedures described in BIOS MCSDK 2.0 user guide to build the csl library. I set the XDC/CG-XML/CCS settings in the pdksetupenv ,and run it under dos command window, then type "xdc",it appears that:

  .../can't open  ./package.xdc.

.../XDC/bld/xdc_rules.mak:372:*** the directory .../pdk_c6678_.../package/ti/drv doesn't contain a buildable package. the package build script package.bld  is missing.stop.

 

 

I guess it means the ccs has problems,but I install it without errors.and I tried to uninstall and reinstall it many times,csl functions in project still can not be recognized. I have done this before with CCSV4.2,and succefully it can recognize the csl functions.

is there anyone help me with it ? thank you very much.