This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI engineers,
We are trying to bring up the board with SoC TDA4VM SR1.1 HS-FS, We using HLOS SBL boot flow, but when running into the SBL, an error "TIFS load...FAILED" was occured.
The tifs.bin we are using from the path: "cp pdk_jacinto_08_04_00_21/packages/ti/drv/sciclient/soc/V1/tifs.bin"
Our SDK version:
LINUX SDK: 08_04_00_11
RTOS SDK: 08_04_00_06
Can you give me some guide to fix this problem?
BRs,
Tahm
Hi Xie,
The booting of HS-FS devices is not supported in SDK 8.4. You need to move to the latest 9.x SDK (9.1+) for HS-FS support on J721E SR1.1 SoCs.
The tifs.bin is the TIFS binary for a GP device. The HS-FS binary for J721E SR1.1 SoCs has a file name of tifs_sr1.1-hs-fs-enc.bin in the packaged SDK. It needs to be copied over as tifs.bin onto your SDCard/eMMC partition, or flashed in the same position as you would for a tifs.bin binary.
regards
Suman
Hi Xie,
I recommend you to move to the latest SDK if the intention is to keep the devices in HS-FS state only, but still have the device booted regularly.
The older SDKs only supported GP and HS-SE. The technical debt is very high to add HS-FS support onto older SDKs.
regards
Suman
Hi,Suman,
Thanks for your response.
Our mass-produced project is based on 8.4 SDK, so we really hope to support HS-FS devices on this SDK version, otherwise it may increase our development cycle and project milestones are not allowed. Please help to see if there is a solution
Regards,
Tahm
Hi Xie,
Can I burn the TI dummy key into an HS-FS device through keywriter and convert it into HS-SE-TIDK device?
Yes
Does 8.4 SDK support TI-SE-TIDK devices?
Yes.
regards
Suman
Hi, Suman,
I refer to this document: https://www.ti.com/lit/pdf/sprad04?keyMatch=HS-FS
and get ti_fek_public.pem from ti fae, after compile keywriter app, i have several questions:
1 which file should I use to burn:
2 How to flash the keywriter file when the system is not boot
3 How to control the voltage VPP_CORE and VPP_MCU when flashing the keywritter?
BRs,
Tahm
Hi Xie,
Please open a new ticket for KeyWriter related queries. This is deviating from the original thread title.
Please look through the corresponding OTP KeyWriter documentation in the PDK Documentation of the RTOS SDK.
regards
Suman