Other Parts Discussed in Thread: SYSBIOS
Hi all,
I've a problem with configuring the gpio driver package. I want to use this package together with the spi driver. I've used the configuration of the example application provided by the PSP package as a template and stripped it down to my needs. Now when running configuro it fails giving me the following error message:
error: ti.psp.gpio.Gpio: "D:/Programme/TI/pspdrivers_02_10_01/packages/ti/psp/gpio/Gpio.xs", line 82: ti.psp.gpio.Gpio.Instance#1 : gpio with instNum =0 in Use
What does this error message mean, and more important how can I get rid of it? I've attached my cfg file, so that you can have a look at my configuration.
Any help on this issue would be very appreciated.
Thanks,
Steve
P.S. The PSP version Iam using is 02_10_01 and sysbios version is 6_30_03_46. If you need additional info, please let me know.